Microchip® Advanced Software Framework

sha204_i2c.c File Reference
#include "conf_twim.h"
#include "conf_atsha204.h"
#include "twi_master.h"
#include "sha204_physical.h"
#include "sha204_lib_return_codes.h"
#include "sha204_timer.h"

Enumerations

enum  i2c_word_address {
  SHA204_I2C_PACKET_FUNCTION_RESET,
  SHA204_I2C_PACKET_FUNCTION_SLEEP,
  SHA204_I2C_PACKET_FUNCTION_IDLE,
  SHA204_I2C_PACKET_FUNCTION_NORMAL
}
 This enumeration lists all packet types sent to a SHA204 device. More...
 

Functions

uint8_t sha204p_idle (void)
 This I2C function puts the SHA204 device into idle state. More...
 
void sha204p_init (void)
 This function initializes peripherals (timer and communication). More...
 
uint8_t sha204p_receive_response (uint8_t size, uint8_t *response)
 This I2C function receives a response from the SHA204 device. More...
 
uint8_t sha204p_reset_io (void)
 This I2C function resets the I/O buffer of the SHA204 device. More...
 
uint8_t sha204p_resync (uint8_t size, uint8_t *response)
 This I2C function resynchronizes communication. More...
 
static uint8_t sha204p_send (uint8_t word_address, uint8_t count, uint8_t *buffer)
 This function sends a I2C packet enclosed by a I2C start and stop to a SHA204 device. More...
 
uint8_t sha204p_send_command (uint8_t count, uint8_t *command)
 This I2C function sends a command to the device. More...
 
void sha204p_set_device_id (uint8_t id)
 This I2C function sets the I2C address. More...
 
uint8_t sha204p_sleep (void)
 This I2C function puts the SHA204 device into low-power state. More...
 
uint8_t sha204p_wakeup (void)
 This I2C function generates a Wake-up pulse and delays. More...
 

Variables

static uint8_t device_address = SHA204_I2C_DEFAULT_ADDRESS >> 1
 I2C address can be changed by calling sha204p_set_device_id. More...
 

This enumeration lists all packet types sent to a SHA204 device.

The following byte stream is sent to a SHA204 TWI device: {I2C start} {I2C address} {word address} [{data}] {I2C stop}. Data are only sent after a word address of value SHA204_I2C_PACKET_FUNCTION_NORMAL.

Enumerator
SHA204_I2C_PACKET_FUNCTION_RESET 

Reset device.

SHA204_I2C_PACKET_FUNCTION_SLEEP 

Put device into Sleep mode.

SHA204_I2C_PACKET_FUNCTION_IDLE 

Put device into Idle mode.

SHA204_I2C_PACKET_FUNCTION_NORMAL 

Write / evaluate data that follow this word address byte.

static uint8_t sha204p_send ( uint8_t  word_address,
uint8_t  count,
uint8_t *  buffer 
)
static

This function sends a I2C packet enclosed by a I2C start and stop to a SHA204 device.

    This function combines a I2C packet send sequence that is common to all packet types.
    Only if word_address is \ref SHA204_I2C_PACKET_FUNCTION_NORMAL, count and buffer parameters are
    expected to be non-zero.
Parameters
[in]word_addresspacket function code listed in i2c_word_address
[in]countnumber of bytes in data buffer
[in]bufferpointer to data buffer
Returns
status of the operation

References ATSHA204_TWI_PORT, twi_package_t::chip, device_address, SHA204_COMM_FAIL, SHA204_SUCCESS, and twi_master_write().

Referenced by sha204p_idle(), sha204p_reset_io(), sha204p_send_command(), and sha204p_sleep().

uint8_t device_address = SHA204_I2C_DEFAULT_ADDRESS >> 1
static

I2C address can be changed by calling sha204p_set_device_id.

Referenced by sha204p_receive_response(), sha204p_send(), and sha204p_set_device_id().