This is the common API for TWIHS.
Additional features are available in the documentation of the specific modules.
See Quickstart guide for Common service TWIHS.
The TWIHS API is partially chip- or platform-specific. While all platforms provide mostly the same functionality, there are some variations around how different bus types and clock tree structures are handled.
The following functions are available on all platforms, but there may be variations in the function signature (i.e. parameters) and behaviour. These functions are typically called by platform-specific parts of drivers, and applications that aren't intended to be portable:
Additional features are available in the documentation of the specific modules.
The twihs API is partially chip- or platform-specific. While all platforms provide mostly the same functionality, there are some variations around how different bus types and clock tree structures are handled.
The following functions are available on all platforms, but there may be variations in the function signature (i.e. parameters) and behaviour. These functions are typically called by platform-specific parts of drivers, and applications that aren't intended to be portable:
Typedefs | |
typedef Twihs * | twihs_master_t |
This type can be used independently to refer to TWIHS master module for the architecture used. More... | |
typedef Twihs * | twihs_slave_t |
This type can be used independently to refer to TWIHS slave module for the architecture used. More... | |
This type can be used independently to refer to TWIHS master module for the architecture used.
It refers to the correct type definition for the architecture.
This type can be used independently to refer to TWIHS slave module for the architecture used.