Files | |
file | mrepeat.h |
Preprocessor macro repeating utils. | |
Macros | |
#define | ASTRINGZ(x) STRINGZ(x) |
Absolute stringize. More... | |
#define | STRINGZ(x) #x |
Stringize. More... | |
#define ASTRINGZ | ( | x | ) | STRINGZ(x) |
Absolute stringize.
Stringize a preprocessing token, this token being allowed to be #defined.
No restriction of use if the token is #defined.
For example, writing ASTRINGZ(PIN0) anywhere with PIN0 #defined as A0 is equivalent to writing "A0".
#define STRINGZ | ( | x | ) | #x |
Stringize.
Stringize a preprocessing token, this token being allowed to be #defined.
May be used only within macros with the token passed as an argument if the token is #defined.
For example, writing STRINGZ(PIN) within a macro #defined by PIN_NAME(PIN) and invoked as PIN_NAME(PIN0) with PIN0 #defined as A0 is equivalent to writing "A0".