Board configuration.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | CONF_BOARD_COM_PORT |
Enable Com Port. More... | |
#define | CONF_BOARD_SPI |
Enable the SPI PINs. More... | |
#define | CONF_BOARD_SPI_NPCS2 |
#define | DATA_FLASH_LED_EXAMPLE_0 LED0 |
LED used for the example. More... | |
#define | DATA_FLASH_LED_EXAMPLE_1 LED0 |
#define CONF_BOARD_COM_PORT |
Enable Com Port.
#define CONF_BOARD_SPI |
Enable the SPI PINs.
#define CONF_BOARD_SPI_NPCS2 |
#define DATA_FLASH_LED_EXAMPLE_0 LED0 |
LED used for the example.
#define DATA_FLASH_LED_EXAMPLE_1 LED0 |