Listen interval.
It is the value of the Wi-Fi STA listen interval for power saving. It is given in units of Beacon period. Periodically after the listen interval fires, the STA is wakeup requesting any buffered frames for it from the AP (Ps-POLL).
#include <m2m_types.h>
Data Fields | |
uint8 | __PAD__ [PAD_SZ(2)] |
uint16 | u16LsnInt |
uint16 tstrM2mLsnInt::u16LsnInt |
Listen interval in Beacon period count.
Referenced by m2m_wifi_set_lsn_int().