Synchronous M2M event handler function, responsible for handling interrupts received from the WILC firmware.
Application developers should call this function periodically in-order to receive the events that are to be handled by the callback functions implemented by the application.
Functions | |
NMI_API sint8 | m2m_wifi_handle_events (void *arg) |
References hif_handle_isr().
Referenced by os_hif_task().