Asynchronous connection status retrieval function, retrieves the status information of the currently connected AP.
Asynchronous associated status retrieval function in the AP mode, retrieves the status information of the currently connected connected stations to the WILC1000 AP.
The result is passed to the Wi-Fi notification callback through the event M2M_WIFI_RESP_CONN_INFO. Connection information is retrieved from the structure tstrM2MConnInfo.
The result is passed to the Wi-Fi notification callback through the event M2M_WIFI_RESP_AP_ASSOC_INFO. Connection information is retrieved from the structure tstrM2MAPAssocInfo.
Functions | |
NMI_API sint8 | m2m_wifi_ap_get_assoc_info (void) |
Request the status information of the currently connected stations to the WILC1000 AP. The result is passed to the Wi-Fi notification callback with the event M2M_WIFI_RESP_AP_ASSOC_INFO. More... | |
NMI_API sint8 | m2m_wifi_get_connection_info (void) |
Request the status information of the currently connected Wi-Fi AP. The result is passed to the Wi-Fi notification callback with the event M2M_WIFI_RESP_CONN_INFO. More... | |
Request the status information of the currently connected stations to the WILC1000 AP. The result is passed to the Wi-Fi notification callback with the event M2M_WIFI_RESP_AP_ASSOC_INFO.
The code snippet shows an example of how wi-fi connection information is retrieved .
References hif_send(), M2M_REQ_GRP_WIFI, M2M_SUCCESS, M2M_WIFI_REQ_AP_ASSOC_INFO, and NULL.
Referenced by os_m2m_wifi_ap_get_assoc_info().
Request the status information of the currently connected Wi-Fi AP. The result is passed to the Wi-Fi notification callback with the event M2M_WIFI_RESP_CONN_INFO.
The code snippet shows an example of how wi-fi connection information is retrieved .
References hif_send(), M2M_REQ_GRP_WIFI, M2M_WIFI_REQ_GET_CONN_INFO, and NULL.
Referenced by os_m2m_wifi_get_connection_info().