Dynamic pool memory manager.
lwIP has dedicated pools for many structures (netconn, protocol control blocks, packet buffers, ...). All these pools are managed here.
#include "lwip/opt.h"
#include "lwip/memp.h"
#include "lwip/pbuf.h"
#include "lwip/udp.h"
#include "lwip/raw.h"
#include "lwip/tcp_impl.h"
#include "lwip/igmp.h"
#include "lwip/api.h"
#include "lwip/api_msg.h"
#include "lwip/sockets.h"
#include "lwip/tcpip.h"
#include "lwip/sys.h"
#include "lwip/timers.h"
#include "lwip/stats.h"
#include "netif/etharp.h"
#include "lwip/ip_frag.h"
#include "lwip/snmp_structs.h"
#include "lwip/snmp_msg.h"
#include "lwip/dns.h"
#include "lwip/netdb.h"
#include "netif/ppp/ppp.h"
#include "netif/ppp/pppoe.h"
#include "netif/ppp/pppol2tp.h"
#include "lwip/nd6.h"
#include "lwip/ip6_frag.h"
#include "lwip/mld6.h"
#include <string.h>
#include "lwip/memp_std.h"
Data Structures | |
struct | memp |
Macros | |
#define | LWIP_MEMPOOL(name, num, size, desc) LWIP_MEM_ALIGN_SIZE(size), |
#define | LWIP_MEMPOOL(name, num, size, desc) (num), |
#define | LWIP_MEMPOOL(name, num, size, desc) (desc), |
#define | LWIP_MEMPOOL(name, num, size, desc) + ( (num) * (MEMP_SIZE + MEMP_ALIGN_SIZE(size) ) ) |
#define | MEMP_ALIGN_SIZE(x) (LWIP_MEM_ALIGN_SIZE(x)) |
#define | MEMP_SIZE 0 |
Functions | |
if (memp!=NULL) | |
LWIP_ERROR ("memp_malloc: type < MEMP_MAX",(type< MEMP_MAX), return NULL;) | |
void | memp_free (memp_t type, void *mem) |
Put an element back into its pool. More... | |
void | memp_init (void) |
Initialize this module. More... | |
MEMP_STATS_INC (err, type) | |
void * | SYS_ARCH_DECL_PROTECT (old_level) |
Get an element from a specific pool. More... | |
SYS_ARCH_PROTECT (old_level) | |
SYS_ARCH_UNPROTECT (old_level) | |
Variables | |
else | |
memp = memp_tab[type] | |
static const char * | memp_desc [MEMP_MAX] |
This array holds a textual description of each pool. More... | |
static u8_t | memp_memory [MEM_ALIGNMENT-1#define LWIP_MEMPOOL(name, num, size, desc)] |
This is the actual memory used by the pools (all pools in one big block). More... | |
static const u16_t | memp_num [MEMP_MAX] |
This array holds the number of elements in each pool. More... | |
static const u16_t | memp_sizes [MEMP_MAX] |
This array holds the element sizes of each pool. More... | |
static struct memp * | memp_tab [MEMP_MAX] |
This array holds the first free element of each pool. More... | |
#define LWIP_MEMPOOL | ( | name, | |
num, | |||
size, | |||
desc | |||
) | LWIP_MEM_ALIGN_SIZE(size), |
#define LWIP_MEMPOOL | ( | name, | |
num, | |||
size, | |||
desc | |||
) | (num), |
#define LWIP_MEMPOOL | ( | name, | |
num, | |||
size, | |||
desc | |||
) | (desc), |
#define LWIP_MEMPOOL | ( | name, | |
num, | |||
size, | |||
desc | |||
) | + ( (num) * (MEMP_SIZE + MEMP_ALIGN_SIZE(size) ) ) |
#define MEMP_ALIGN_SIZE | ( | x | ) | (LWIP_MEM_ALIGN_SIZE(x)) |
#define MEMP_SIZE 0 |
Referenced by if(), memp_free(), and memp_init().
if | ( | memp! | = NULL | ) |
References LWIP_ASSERT, MEM_ALIGNMENT, MEMP_SIZE, MEMP_STATS_INC_USED, memp::next, and NULL.
Referenced by _http_client_handle_entity(), _http_client_read_chuked_entity(), etharp_query(), icmp6_input(), icmp_input(), ip6_input(), ip6_reass(), ip6_reass_free_complete_datagram(), ip_frag(), ip_input(), ip_reass(), ip_reass_chain_frag_into_datagram_and_validate(), ip_reass_free_complete_datagram(), lwip_ioctl(), lwip_netconn_do_writemore(), nd6_input(), nd6_send_rs(), pbuf_header_impl(), raw_input(), status_callback(), and tcp_zero_window_probe().
LWIP_ERROR | ( | ) |
Referenced by dhcp_arp_reply(), dhcp_bind(), dhcp_create_msg(), dhcp_delete_msg(), dhcp_inform(), dhcp_option_trailer(), dhcp_parse_reply(), dhcp_start(), dhcp_stop(), etharp_arp_input(), lwip_bind(), lwip_connect(), lwip_netconn_do_connect(), lwip_sendto(), netbuf_alloc(), netbuf_chain(), netbuf_data(), netbuf_first(), netbuf_free(), netbuf_next(), netbuf_ref(), netconn_accept(), netconn_bind(), netconn_close_shutdown(), netconn_connect(), netconn_disconnect(), netconn_getaddr(), netconn_gethostbyname(), netconn_join_leave_group(), netconn_listen_with_backlog(), netconn_recv(), netconn_recv_data(), netconn_recv_tcp_pbuf(), netconn_send(), netconn_write_partly(), pbuf_cat(), pbuf_copy(), pbuf_copy_partial(), pbuf_header_impl(), pbuf_take(), tcp_bind(), tcp_connect(), tcp_listen_with_backlog(), and tcp_write().
Put an element back into its pool.
type | the pool where to put mem |
mem | the memp element to free |
References LWIP_ASSERT, MEM_ALIGNMENT, memp, MEMP_SIZE, MEMP_STATS_DEC, memp::next, NULL, SYS_ARCH_DECL_PROTECT(), SYS_ARCH_PROTECT(), and SYS_ARCH_UNPROTECT().
Referenced by etharp_query(), etharp_update_arp_entry(), ip6_reass(), ip6_reass_free_complete_datagram(), ip_frag_free_pbuf_custom_ref(), ip_reass_dequeue_datagram(), lwip_freeaddrinfo(), mld6_free_group(), mld6_stop(), nd6_free_q(), nd6_send_q(), netbuf_chain(), netbuf_delete(), netconn_alloc(), netconn_free(), netconn_new_with_proto_and_callback(), netconn_recv(), pbuf_free(), raw_remove(), tcp_abandon(), tcp_close_shutdown(), tcp_input(), tcp_listen_with_backlog(), tcp_seg_free(), tcp_slowtmr(), tcpip_callback_with_block(), tcpip_callbackmsg_delete(), tcpip_input(), tcpip_thread(), and udp_remove().
Initialize this module.
Carves out memp_memory into linked lists for each pool-type.
References LWIP_MEM_ALIGN, max, memp, MEMP_MAX, memp_memory, MEMP_SIZE, memp_sizes, MEMP_STATS_AVAIL, memp::next, and NULL.
Referenced by lwip_init().
MEMP_STATS_INC | ( | err | , |
type | |||
) |
void* SYS_ARCH_DECL_PROTECT | ( | old_level | ) |
Get an element from a specific pool.
type | the pool to get an element from |
the debug version has two more parameters:
file | file name calling this function |
line | number of line where this function is called |
Referenced by alloc_socket(), err_tcp(), event_callback(), free_socket(), lwip_accept(), lwip_select(), lwip_selscan(), memp_free(), pbuf_free(), pbuf_free_ooseq(), pbuf_pool_is_empty(), pbuf_ref(), and sys_thread_new().
SYS_ARCH_PROTECT | ( | old_level | ) |
SYS_ARCH_UNPROTECT | ( | old_level | ) |
else |
Referenced by memp_free(), and memp_init().
|
static |
This array holds a textual description of each pool.
|
static |
This is the actual memory used by the pools (all pools in one big block).
Referenced by memp_init().
This array holds the element sizes of each pool.
Referenced by memp_init().