![]() | Copyright (c) 2018 Microchip Technology Inc |
![]() | This is the quick start guide for the PIO Driver, with step-by-step instructions on how to configure and use the driver for specific use cases |
![]() | |
![]() | |
![]() | This is a list of the available Quick Start Guides (QSGs) and example applications for SAMV71/V70/E70/S70 XDMA Controller (XDMAC) Driver |
![]() ![]() | This is the quick start guide for the SAMV71/V70/E70/S70 XDMA Controller (XDMAC) Driver, with step-by-step instructions on how to configure and use the driver for a specific use case.The code examples can be copied into e.g the main application loop or any other function that will need to control the XDMAC module |
![]() | |
![]() | This is the quickstart guide for the SAM SPI driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
![]() | Service (SAMV71) |
![]() | Management (SAMV71) |
![]() | This is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases |
![]() ![]() | In this case we will read out the pins from one whole port and write the read value to another port |
![]() | This is the quick start guide for the Serial Interface module, with step-by-step instructions on how to configure and use the serial in a selection of use cases |
![]() ![]() | In this use case, the USART module is configured for: |
![]() | This is the quick start guide for the USART module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
![]() ![]() | In this use case, the USART module is configured for: |
![]() ![]() | In this use case, the USART module is configured for: |
![]() | This page lists several definition related to the board operating frequency |
![]() | This page lists several definition related to the board description |
![]() | This page lists definitions related to CAN0 and CAN1 |
![]() | |
![]() | |
![]() |