Network buffer management.
Functions | |
void * | netbuf_alloc (struct netbuf *buf, u16_t size) |
Allocate memory for a packet buffer for a given netbuf. More... | |
void | netbuf_chain (struct netbuf *head, struct netbuf *tail) |
Chain one netbuf to another (. More... | |
err_t | netbuf_data (struct netbuf *buf, void **dataptr, u16_t *len) |
Get the data pointer and length of the data inside a netbuf. More... | |
void | netbuf_delete (struct netbuf *buf) |
Deallocate a netbuf allocated by netbuf_new(). More... | |
void | netbuf_first (struct netbuf *buf) |
Move the current data pointer of a packet buffer contained in a netbuf to the beginning of the packet. More... | |
void | netbuf_free (struct netbuf *buf) |
Free the packet buffer included in a netbuf. More... | |
struct netbuf * | netbuf_new (void) |
Create (allocate) and initialize a new netbuf. More... | |
s8_t | netbuf_next (struct netbuf *buf) |
Move the current data pointer of a packet buffer contained in a netbuf to the next part. More... | |
err_t | netbuf_ref (struct netbuf *buf, const void *dataptr, u16_t size) |
Let a netbuf reference existing (non-volatile) data. More... | |
Allocate memory for a packet buffer for a given netbuf.
buf | the netbuf for which to allocate a packet buffer |
size | the size of the packet buffer to allocate |
References LWIP_ASSERT, LWIP_ERROR(), NULL, pbuf_alloc(), pbuf_free(), PBUF_POOL, and PBUF_TRANSPORT.
Referenced by iperf_udp_recv(), and iperf_udp_send().
void netbuf_chain | ( | struct netbuf * | head, |
struct netbuf * | tail | ||
) |
Chain one netbuf to another (.
head | the first netbuf |
tail | netbuf to chain after head, freed by this function, may not be reference after returning |
References LWIP_ERROR(), memp_free(), NULL, and pbuf_cat().
Get the data pointer and length of the data inside a netbuf.
buf | netbuf to get the data from |
dataptr | pointer to a void pointer where to store the data pointer |
len | pointer to an u16_t where the length of the data is stored |
References ERR_ARG, ERR_BUF, ERR_OK, LWIP_ERROR(), and NULL.
Referenced by iperf_tcp_recv(), and iperf_udp_recv().
void netbuf_delete | ( | struct netbuf * | buf | ) |
Deallocate a netbuf allocated by netbuf_new().
buf | pointer to a netbuf allocated by netbuf_new() |
References memp_free(), NULL, and pbuf_free().
Referenced by iperf_tcp_recv(), iperf_udp_recv(), iperf_udp_send(), netconn_drain(), recv_raw(), and recv_udp().
void netbuf_first | ( | struct netbuf * | buf | ) |
Move the current data pointer of a packet buffer contained in a netbuf to the beginning of the packet.
The packet buffer itself is not modified.
buf | the netbuf to modify |
References LWIP_ERROR(), and NULL.
void netbuf_free | ( | struct netbuf * | buf | ) |
Free the packet buffer included in a netbuf.
buf | pointer to the netbuf which contains the packet buffer to free |
References LWIP_ERROR(), NULL, and pbuf_free().
struct netbuf* netbuf_new | ( | void | ) |
Create (allocate) and initialize a new netbuf.
The netbuf doesn't yet contain a packet buffer!
References ipX_addr_set_any, LWIP_IPV6, memp_malloc(), and NULL.
Referenced by iperf_udp_recv(), and iperf_udp_send().
s8_t netbuf_next | ( | struct netbuf * | buf | ) |
Move the current data pointer of a packet buffer contained in a netbuf to the next part.
The packet buffer itself is not modified.
buf | the netbuf to modify |
References LWIP_ERROR(), and NULL.
Let a netbuf reference existing (non-volatile) data.
buf | netbuf which should reference the data |
dataptr | pointer to the data to reference |
size | size of the data |
References ERR_ARG, ERR_MEM, ERR_OK, LWIP_ERROR(), NULL, pbuf_alloc(), pbuf_free(), PBUF_REF, and PBUF_TRANSPORT.