Microchip® Advanced Software Framework

ping.h File Reference

Ping sender module.

#include "lwip/ip_addr.h"

Macros

#define PING_USE_SOCKETS   LWIP_SOCKET
 PING_USE_SOCKETS: Set to 1 to use sockets, otherwise the raw api is used. More...
 

Functions

void ping_function (char *addr, u32_t u32PingCount)
 
void ping_send_now (void)
 

#define PING_USE_SOCKETS   LWIP_SOCKET

PING_USE_SOCKETS: Set to 1 to use sockets, otherwise the raw api is used.

void ping_function ( char *  addr,
u32_t  u32PingCount 
)
void ping_send_now ( void  )