Microchip® Advanced Software Framework

tstrM2MMulticastMac Struct Reference

M2M add/remove multicast mac address.

#include <m2m_types.h>

Data Fields

uint8 __PAD__ [PAD_SZ(M2M_MAC_ADDRES_LEN+1)]
 
uint8 au8macaddress [M2M_MAC_ADDRES_LEN]
 
uint8 u8AddRemove
 

uint8 tstrM2MMulticastMac::__PAD__[PAD_SZ(M2M_MAC_ADDRES_LEN+1)]

Padding bytes for forcing 4-byte alignment

uint8 tstrM2MMulticastMac::au8macaddress[M2M_MAC_ADDRES_LEN]

Mac address needed to be added or removed from filter.

Referenced by m2m_wifi_enable_mac_mcast().

uint8 tstrM2MMulticastMac::u8AddRemove

set by 1 to add or 0 to remove from filter.

Referenced by m2m_wifi_enable_mac_mcast().