License | Subject to your compliance with these terms, you may use Microchip software and any derivatives exclusively with Microchip products |
Extra Information for PORT Driver | |
Examples for PORT Driver | This is a list of the available Quick Start guides (QSGs) and example applications for SAM Port (PORT) Driver |
 Quick Start Guide for PORT - Basic | In this use case, the PORT module is configured for: |
Document Revision History | |
Extra Information for SYSTEM PINMUX Driver | |
Examples for SYSTEM PINMUX Driver | This is a list of the available Quick Start guides (QSGs) and example applications for SAM System Pin Multiplexer (SYSTEM PINMUX) Driver |
 Quick Start Guide for SYSTEM PINMUX - Basic | In this use case, the PINMUX module is configured for: |
Document Revision History | |
Extra Information for SERCOM SPI Driver | |
Examples for SERCOM SPI Driver | This is a list of the available Quick Start guides (QSGs) and example applications for SAM Serial Peripheral Interface (SERCOM SPI) Driver |
 Quick Start Guide for SERCOM SPI Master - Polled | In this use case, the SPI on extension header 1 of the Xplained Pro board will be configured with the following settings: |
 Quick Start Guide for SERCOM SPI Slave - Polled | In this use case, the SPI on extension header 1 of the Xplained Pro board will configured with the following settings: |
 Quick Start Guide for SERCOM SPI Master - Callback | In this use case, the SPI on extension header 1 of the Xplained Pro board will be configured with the following settings: |
 Quick Start Guide for SERCOM SPI Slave - Callback | In this use case, the SPI on extension header 1 of the Xplained Pro board will configured with the following settings: |
 Quick Start Guide for Using DMA with SERCOM SPI | The supported board list: |
MUX Settings | The following lists the possible internal SERCOM module pad function assignments for the four SERCOM pads in both SPI Master and SPI Slave modes |
Document Revision History | |
Extra Information for SYSTEM Driver | |
Document Revision History | |
Extra Information for SYSTEM CLOCK Driver | |
Examples for System Clock Driver | This is a list of the available Quick Start guides (QSGs) and example applications for SAM System Clock Management (SYSTEM CLOCK) Driver |
Document Revision History | |
Extra Information for SYSTEM INTERRUPT Driver | |
Examples for SYSTEM INTERRUPT Driver | This is a list of the available Quick Start guides (QSGs) and example applications for SAM System Interrupt (SYSTEM INTERRUPT) Driver |
Document Revision History | |
Extra Information for EXTINT Driver | |
Examples for EXTINT Driver | This is a list of the available Quick Start guides (QSGs) and example applications for SAM External Interrupt (EXTINT) Driver |
Document Revision History | |
Extra Information for ADC Driver | |
Examples for ADC Driver | This is a list of the available Quick Start guides (QSGs) and example applications for SAM Analog-to-Digital Converter (ADC) Driver |
Document Revision History | |
Extra Information for TCC Driver | |
Examples for TCC Driver | This is a list of the available Quick Start guides (QSGs) and example applications for SAM Timer Counter for Control Applications (TCC) Driver |
 Quick Start Guide for TCC - Basic | The supported board list: |
 Quick Start Guide for TCC - Double Buffering and Circular | The supported board list: |
 Quick Start Guide for TCC - Timer | The supported board list: |
 Quick Start Guide for TCC - Callback | The supported board list: |
 Quick Start Guide for TCC - Non-Recoverable Fault | The supported kit list: |
 Quick Start Guide for TCC - Recoverable Fault | The supported board list: |
 Quick Start Guide for Using DMA with TCC | The supported board list: |
Document Revision History | |
Extra Information for RTC (CAL) Driver | |
Examples for RTC CAL Driver | This is a list of the available Quick Start guides (QSGs) and example applications for SAM RTC Calendar (RTC CAL) Driver |
Document Revision History | |
Quick Start Guide for the SAM AT30TSE75X Temperature Sensor Driver | In this use case we will interface the temperature sensor, set a resolution and read the temperature |
Extra Information for SERCOM I2C Driver | |
Examples for SERCOM I2C Driver | This is a list of the available Quick Start guides (QSGs) and example applications for Asfdoc_sam0_sercom_i2c_group |
Document Revision History | |
Quick Start Guide for SERCOM I2C Master - Basic | In this use case, the I2C will used and set up as follows: |
Quick Start Guide for SERCOM I2C Master - Callback | In this use case, the I2C will used and set up as follows: |
Quick Start Guide for Using DMA with SERCOM I2C Master | The supported board list: |
Quick start guide for Serial Interface service | This is the quick start guide for the Serial Interface module, with step-by-step instructions on how to configure and use the serial in a selection of use cases |
 Advanced use case - Send a packet of serial data | In this use case, the USART module is configured for: |
Extra Information for SERCOM USART Driver | |
Examples for SERCOM USART Driver | This is a list of the available Quick Start guides (QSGs) and example applications for SAM Serial USART (SERCOM USART) Driver |
 Quick Start Guide for SERCOM USART - Basic | This quick start will echo back characters typed into the terminal |
 Quick Start Guide for SERCOM USART - Callback | This quick start will echo back characters typed into the terminal, using asynchronous TX and RX callbacks from the USART peripheral |
 Quick Start Guide for Using DMA with SERCOM USART | The supported board list: |
 Quick Start Guide for SERCOM USART LIN | The supported board list: |
SERCOM USART MUX Settings | The following lists the possible internal SERCOM module pad function assignments, for the four SERCOM pads when in USART mode |
Document Revision History | |