Microchip® Advanced Software Framework

sockaddr_in Struct Reference

Socket address structure for IPV4 addresses. Used to specify socket address information to connect to. Can be cast to sockaddr structure.

#include <socket.h>

Data Fields

in_addr sin_addr
 
uint16 sin_family
 
uint16 sin_port
 
uint8 sin_zero [8]
 

in_addr sockaddr_in::sin_addr

IP Address of the socket. The IP address is of type in_addr structure. Can be set to "0" to accept any IP address for server operation.

Referenced by handle_dns_found(), handle_start_connect(), m2m_ip_cb(), sendto(), and setup_android_sockets().

uint16 sockaddr_in::sin_family

Specifies the address family(AF). Members of AF_INET address family are IPv4 addresses. Hence,the only supported value for this is AF_INET.

Referenced by handle_start_connect(), m2m_ip_cb(), sendto(), and setup_android_sockets().

uint16 sockaddr_in::sin_port

Port number of the socket. Network sockets are identified by a pair of IP addresses and port number. It must be set in the Network Byte Order format , _htons (e.g. _htons(80)). Can NOT have zero value.

Referenced by handle_start_connect(), m2m_ip_cb(), sendto(), and setup_android_sockets().

uint8 sockaddr_in::sin_zero[8]

Padding to make structure the same size as sockaddr.