The following list of macros are used to define constants used throughout the socket layer.
Macros | |
#define | AF_INET 2 |
#define | HOSTNAME_MAX_SIZE 64 |
#define | IP_ADD_MEMBERSHIP 0x01 |
#define | IP_DROP_MEMBERSHIP 0x02 |
#define | MAX_SOCKET (TCP_SOCK_MAX + UDP_SOCK_MAX) |
#define | SO_SET_UDP_SEND_CALLBACK 0x00 |
#define | SO_TCP_KEEPALIVE 0x04 |
#define | SO_TCP_KEEPCNT 0x07 |
#define | SO_TCP_KEEPIDLE 0x05 |
#define | SO_TCP_KEEPINTVL 0x06 |
#define | SOCK_DGRAM 2 |
#define | SOCK_STREAM 1 |
#define | SOCKET_BUFFER_MAX_LENGTH 1400 |
#define | SOCKET_CONFIG_SSL_DELAY 2 |
#define | SOCKET_CONFIG_SSL_OFF 0 |
#define | SOCKET_CONFIG_SSL_ON 1 |
#define | SOCKET_FLAGS_SSL 0x01 |
#define | SOL_SOCKET 1 |
#define | SOL_SSL_SOCKET 2 |
#define | TCP_SOCK_MAX (7) |
#define | UDP_SOCK_MAX 4 |
#define AF_INET 2 |
The AF_INET is the address family used for IPv4. An IPv4 transport address is specified with the sockaddr_in structure. (It is the only supported type for the current implementation.)
Referenced by demo_start(), m2m_ip_cb(), and socket().
#define HOSTNAME_MAX_SIZE 64 |
Maximum allowed size for a host domain name passed to the function gethostbyname gethostbyname. command value. Used with the setsockopt function.
Referenced by gethostbyname(), and sslSetSockOpt().
#define IP_ADD_MEMBERSHIP 0x01 |
Set Socket Option Add Membership command value (to join a multicast group). Used with the setsockopt function.
#define IP_DROP_MEMBERSHIP 0x02 |
Set Socket Option Drop Membership command value (to leave a multicast group). Used with the setsockopt function.
#define MAX_SOCKET (TCP_SOCK_MAX + UDP_SOCK_MAX) |
Maximum number of simultaneous sockets.
Referenced by accept(), bind(), close(), connect(), listen(), m2m_ip_cb(), recv(), recvfrom(), secure(), send(), sendto(), setsockopt(), socketDeinit(), and socketInit().
#define SO_SET_UDP_SEND_CALLBACK 0x00 |
Socket option used by the application to enable/disable the use of UDP send callbacks.
Used with the setsockopt function.
The option value should be cast to int type.
0: disable UDP send callbacks.
1: enable UDP send callbacks.
Default setting is enable.
Referenced by demo_start().
#define SO_TCP_KEEPALIVE 0x04 |
Socket option to enable or disable TCP keep-alive.
Used with the setsockopt function.
The option value should be cast to int type.
0: disable TCP keep-alive.
1: enable TCP keep-alive.
Default setting is disable.
#define SO_TCP_KEEPCNT 0x07 |
Socket option to set the number of keep-alive retransmissions to be carried out before declaring that the remote end is not available.
Used with the setsockopt function.
The option value should be cast to int type.
Maximum 255. Default setting is 20.
#define SO_TCP_KEEPIDLE 0x05 |
Socket option to set the time period after which the socket will trigger keep-alive transmissions.
Used with the setsockopt function.
The option value should be cast to int type.
Option value is the time period in units of 500ms. Maximum 2^32 - 1. Default setting is 120 (60 seconds).
#define SO_TCP_KEEPINTVL 0x06 |
Socket option to set the time period between keep-alive retransmissions.
Used with the setsockopt function.
The option value should be cast to int type.
Option value is the time period in units of 500ms. Maximum 255. Default setting is 1 (0.5 seconds).
#define SOCK_DGRAM 2 |
One of the IPv4 supported socket types for unreliable connectionless datagram connection. Passed to the socket function for the socket creation operation.
Referenced by demo_start(), and socket().
#define SOCK_STREAM 1 |
#define SOCKET_BUFFER_MAX_LENGTH 1400 |
#define SOCKET_CONFIG_SSL_DELAY 2 |
#define SOCKET_CONFIG_SSL_OFF 0 |
#define SOCKET_CONFIG_SSL_ON 1 |
This value may be passed in the u8Config parameter of socket, to create a TLS socket.
Note that the number of TLS sockets is limited to 4.
#define SOCKET_FLAGS_SSL 0x01 |
This flag may be set in the u8Config parameter of socket, to create a TLS socket.
Note that the number of TLS sockets is limited to 4.
This flag is kept for legacy purposes. It is recommended that applications use SOCKET_CONFIG_SSL_ON instead.
#define SOL_SOCKET 1 |
Socket option. Used with the setsockopt function
Referenced by demo_start(), and setsockopt().
#define SOL_SSL_SOCKET 2 |
SSL Socket option level. Used with the setsockopt function
Referenced by set_alpn_list(), and setsockopt().
#define TCP_SOCK_MAX (7) |
Maximum number of simultaneous TCP sockets.
Referenced by get_alpn_index(), get_error_detail(), send(), set_alpn_list(), socket(), and sslSetSockOpt().
#define UDP_SOCK_MAX 4 |
Maximum number of simultaneous UDP sockets.
Referenced by socket().