Functions | |
NMI_API sint8 | m2m_ota_abort (void) |
Request OTA Abort. More... | |
NMI_API sint8 | m2m_ota_init (tpfOtaUpdateCb pfOtaUpdateCb, tpfOtaNotifCb pfOtaNotifCb) |
Initialize the OTA layer. More... | |
sint8 m2m_ota_abort | ( | void | ) |
Request OTA Abort.
Request the WINC to abort an OTA or Host File download in progress.
If no download is in progress, the API will respond with failure.
References hif_send(), M2M_OTA_REQ_ABORT, M2M_REQ_GROUP_OTA, M2M_SUCCESS, and NULL.
sint8 m2m_ota_init | ( | tpfOtaUpdateCb | pfOtaUpdateCb, |
tpfOtaNotifCb | pfOtaNotifCb | ||
) |
Initialize the OTA layer.
Synchronous initialization function for the OTA layer by registering the update callback.
The notification callback is not supported at the current version. Calling this API is a MUST for all the OTA API's.
[in] | pfOtaUpdateCb | OTA Update callback function. |
[in] | pfOtaNotifCb | OTA Notify callback function. |
[in] | pfOtaUpdateCb | OTA Update callback function. |
[in] | pfOtaNotifCb | OTA Notify callback function. |
References gpfOtaNotifCb, gpfOtaUpdateCb, hif_register_cb(), hif_send(), M2M_ERR, m2m_ota_cb(), M2M_OTA_REQ_HOST_FILE_STATUS, M2M_REQ_GROUP_OTA, M2M_SUCCESS, and NULL.