Introduction
This example demonstrates the use of the WINC1500 with the SAMx2x Xplained Pro board to connect to a secured 802.1x enterprise network that supports TLS as phase 2 authentication.
The following Enterprise security methods are supported by this example.
* - EAP with TLS
* - PEAPv0 with TLS
* - PEAPv1 with TLS
*
It uses the following hardware:
- the SAM Xplained Pro.
- the WINC1500 on EXT1.
Main Files
- main.c : Initialize the WINC1500 and connect to network that support enterprise security with TLS authentication protocol.
Usage
- Assemble the devices and connect to USB debug cable from PC.
- On the computer, open and configure a terminal application as the follows.
* Baud Rate : 115200
* Data : 8bit
* Parity bit : none
* Stop bit : 1bit
* Flow control : none
*
- Prepare an AP that supports enterprise security with any of the following security method.
- EAP with TLS
- PEAPv0 with TLS
- PEAPv1 with TLS
- You need to know following things before configuring RADIUS server settings in the AP. Ask your network administrator to get there information and configure it in the WINC1500.
* User name
* Name of wireless network
*
- Modify MAIN_WLAN_802_1X_USR_NAME to the user name.
- Modify the python script key_decoder.py available in the script folder with path to user certificate and key file. Execute the script to generate the file privateKey_decoded.txt which contain the certificate and private key coefficient. Copyt the content of privateKey_decoded.txt and update the arrays modulus, exponent and certificate in main.h file. Modify MAIN_WLAN_SSID to wireless network name
- Build and run the application. If the device connected successfully, IP address which is assigned by DHCP will be displayed on the terminal program.
* -- WINC1500 enterprise security connection with TLS example --
* -- SAMXXX_XPLAINED_PRO --
* -- Compiled: xxx xx 2021 hh:mm:ss --
* (APP)(INFO)Chip ID xxxxxx
* (APP)(INFO)DriverVerInfo: 0xaaaaaaaa
* (APP)(INFO)Firmware ver : xx.x.x xxxxxx xxxxx
* (APP)(INFO)Firmware Build xxx xx xxxx xx:xx:xx
* (APP)(INFO)Firmware
Min driver ver : xx.x.x
* (APP)(INFO)Driver ver: xx.x.x
* (APP)(INFO)Driver built at xxx xx xxxx xx:xx:xx
* Username:DEMO_USER
* Connecting to WINC1500_ENTERPRISE...
* Username:DEMO_USER
* Wi-Fi connected
* Wi-Fi IP is xxx.xxx.xxx.xxx
* Connection successfully completed.
*
- Warning
* For
using the security enterprise network, the root
certificate must be written to WINC1500.
* Download the root
certificate using the root_certificate_downloader. (Refer to WINC1500 Software User Guide.)
*
Compilation Information
This software was written for the GNU GCC compiler using Atmel Studio 6.2 Other compilers may or may not work.
Contact Information
For further information, visit Microchip.