#include <m2m_wifi.h>
bool tstrAuth1xTls::bPrependDomain |
Determines whether Domain is prepended or appended to UserName in EAP identity responses. true: Domain is prepended to UserName - [Domain][UserName]. false: Domain is appended to UserName - [UserName][Domain].
Referenced by m2m_wifi_connect_1x_tls(), and wifi_ap_connect().
bool tstrAuth1xTls::bUnencryptedUserName |
Determines whether UserName or "anonymous" is sent (unencrypted) in the initial EAP identity response. Domain is sent in both cases.
true: UserName is sent in the initial EAP identity response (required for EAP-TLS). false: "anonymous" is sent in the initial EAP identity response. This setting is recommended for tunneled methods such as EAP-PEAP/TLS.
Referenced by m2m_wifi_connect_1x_tls(), and wifi_ap_connect().
uint8* tstrAuth1xTls::pu8Certificate |
Pointer to TLS client certificate corresponding to PrivateKey. This will be used during TLS client authentication.
Referenced by m2m_wifi_connect_1x_tls(), post_main_page(), and wifi_ap_connect().
uint8* tstrAuth1xTls::pu8Domain |
Pointer to Domain of authentication server (printable ASCII), including '@' or '\' separator character as appropriate. Use NULL if there is no domain information. The Domain will be either prepended or appended to the UserName, depending on the setting of field bPrependDomain.
Example 1: if [Domain]is "@my_domain" and bPrependDomain is false, then the EAP identity response is "[UserName]@my_domain".
Example 2: if [Domain]is "my_domain\" and bPrependDomain is true, then the EAP identity response is "my_domain\[UserName]".
Referenced by m2m_wifi_connect_1x_tls(), and wifi_ap_connect().
uint8* tstrAuth1xTls::pu8PrivateKey_Exp |
Pointer to PrivateKey exponent (raw data). This will be used during TLS client authentication.
Referenced by m2m_wifi_connect_1x_tls(), post_main_page(), and wifi_ap_connect().
uint8* tstrAuth1xTls::pu8PrivateKey_Mod |
Pointer to PrivateKey modulus (raw data). This will be used during TLS client authentication.
Referenced by m2m_wifi_connect_1x_tls(), post_main_page(), and wifi_ap_connect().
uint8* tstrAuth1xTls::pu8UserName |
Pointer to UserName (ASCII). This will be sent (encrypted) in the tunneled EAP identity response. If bUnencryptedUserName is true then it will also be sent (unencrypted) in the initial EAP identity response.
Referenced by m2m_wifi_connect_1x_tls(), post_main_page(), and wifi_ap_connect().
uint16 tstrAuth1xTls::u16CertificateLen |
Length of Certificate (in bytes). Permitted values are between 0 and M2M_AUTH_1X_CERT_LEN_MAX.
Referenced by m2m_wifi_connect_1x_tls(), post_main_page(), and wifi_ap_connect().
uint16 tstrAuth1xTls::u16DomainLen |
Length of Domain (in ASCII characters), including '@' or '\' separator character as appropriate. Permitted values are such that u16DomainLen + u16UserNameLen is between 0 and M2M_AUTH_1X_USER_LEN_MAX.
Referenced by m2m_wifi_connect_1x_tls().
uint16 tstrAuth1xTls::u16PrivateKeyLen |
Length of PrivateKey_Mod (in bytes). Permitted values are between 0 and M2M_AUTH_1X_PRIVATEKEY_LEN_MAX, typically 128 or 256. PrivateKey_Exp must be the same length as modulus, pre-padded with 0s if necessary.
Referenced by m2m_wifi_connect_1x_tls(), post_main_page(), and wifi_ap_connect().
uint16 tstrAuth1xTls::u16UserNameLen |
Length of UserName (in ASCII characters). Permitted values are such that u16DomainLen + u16UserNameLen is between 0 and M2M_AUTH_1X_USER_LEN_MAX.
Referenced by m2m_wifi_connect_1x_tls(), and wifi_ap_connect().