WINC1500 Security Connection with Wi-Fi Protected Setup(WPS) Example.
Copyright (c) 2016-2018 Microchip Technology Inc. and its subsidiaries.
#include "asf.h"
#include "main.h"
#include "driver/include/m2m_wifi.h"
#include "driver/source/nmasic.h"
Macros | |
#define | STRING_EOL "\r\n" |
#define | STRING_HEADER |
Functions | |
static void | btn_init (void) |
Initialize buttons driver. More... | |
static void | btn_press (uint8_t btn, uint8_t press) |
button pressed callback function. More... | |
static void | configure_console (void) |
Configure UART console. More... | |
int | main (void) |
Main application function. More... | |
static void | wifi_cb (uint8_t u8MsgType, void *pvMsg) |
Callback to get the Wi-Fi status update. More... | |
Variables | |
static struct usart_module | cdc_uart_module |
UART module for debug. More... | |
static bool | gbPressButton = false |
#define STRING_EOL "\r\n" |
#define STRING_HEADER |
Referenced by main().
|
static |
Initialize buttons driver.
References btn_press(), BUTTON_0_ACTIVE, BUTTON_0_PIN, gbPressButton, MAIN_SW1, and port_pin_get_input_level().
Referenced by main().
|
static |
button pressed callback function.
References m2m_wifi_wps(), MAIN_SW1, NULL, and WPS_PBC_TRIGGER.
Referenced by btn_init().
|
static |
Configure UART console.
References usart_config::baudrate, cdc_uart_module, EDBG_CDC_MODULE, EDBG_CDC_SERCOM_MUX_SETTING, EDBG_CDC_SERCOM_PINMUX_PAD0, EDBG_CDC_SERCOM_PINMUX_PAD1, EDBG_CDC_SERCOM_PINMUX_PAD2, EDBG_CDC_SERCOM_PINMUX_PAD3, usart_config::mux_setting, usart_config::pinmux_pad0, usart_config::pinmux_pad1, usart_config::pinmux_pad2, usart_config::pinmux_pad3, usart_enable(), and usart_get_config_defaults().
Referenced by main().
int main | ( | void | ) |
Main application function.
Application entry point. Initialize system, UART and board specific settings. Connect AP using WPS.
References btn_init(), configure_console(), gbPressButton, M2M_SUCCESS, m2m_wifi_handle_events(), m2m_wifi_init(), m2m_wifi_set_device_name(), m2m_wifi_wps(), MAIN_WPS_PIN_NUMBER, MAIN_WPS_PUSH_BUTTON_FEATURE, nm_bsp_init(), NULL, tstrWifiInitParam::pfAppWifiCb, STRING_HEADER, system_init(), wifi_cb(), and WPS_PIN_TRIGGER.
|
static |
Callback to get the Wi-Fi status update.
[in] | u8MsgType | type of Wi-Fi notification. Possible types are: |
[in] | pvMsg | A pointer to a buffer containing the notification parameters (if any). It should be casted to the correct data type corresponding to the notification type. |
References tstrM2MWPSInfo::au8PSK, tstrM2MWPSInfo::au8SSID, m2m_strlen(), M2M_WIFI_CH_ALL, m2m_wifi_connect(), M2M_WIFI_CONNECTED, M2M_WIFI_DISCONNECTED, M2M_WIFI_REQ_DHCP_CONF, M2M_WIFI_REQ_WPS, m2m_wifi_request_dhcp_client(), m2m_wifi_request_scan(), M2M_WIFI_RESP_CON_STATE_CHANGED, tstrM2MWPSInfo::u8AuthType, tstrM2MWPSInfo::u8Ch, and tstrM2mWifiStateChanged::u8CurrState.
Referenced by main().
|
static |
UART module for debug.
Referenced by configure_console().
Referenced by btn_init(), and main().