Synchronous function which returns a BSD socket compliant Internet Protocol (IPv4) socket address.
This IPv4 address in the input string parameter could either be specified as a host name, or as a numeric string representation like n.n.n.n known as the IPv4 dotted-decimal format (i.e. "192.168.10.1"). This function is used whenever an ip address needs to be set in the proper format (i.e. for the tstrM2MIPConfig structure).
Functions | |
NMI_API uint32 | nmi_inet_addr (char *pcIpAddr) |
[in] | pcIpAddr | A null terminated string containing the IP address in IPv4 dotted-decimal address. |
References m2m_memcpy().
Referenced by connect_cmd_handler().