Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Modules
Here is a list of all modules:
[detail level 123]
oWINC1500 (Wi-Fi)
oStandard I/O (stdio)Common standard I/O driver that implements the stdio read and write functions on AVR and SAM devices
|\Standard serial I/O (stdio)Common standard serial I/O management driver that implements a stdio serial interface on AVR and SAM devices
oBSP
Description of the BSP (<strong>B</strong>oard <strong>S</strong>upport <strong>P</strong>ackage) module.
|oData Types
|oDefines
|\Functions
    Lists the available BSP (<strong>B</strong>oard <strong>S</strong>upport <strong>P</strong>ackage) APIs.
oCommon
|oDefines
|\Functions
oOTA
 The WINC supports OTA (Over-The-Air) updates.
|oCallbacks
     Lists the different callbacks that can be used during OTA updates.
|oDefines
     Specifies the macros and defines used by the OTA APIs.
|oEnumerations and Typedefs
     Specifies the enums and Data Structures used by the OTA APIs.
|\Functions
     Lists the full set of available APIs to manage OTA updates and Host File Downloads.
oSSL
 Provides a description of the SSL Layer.
|oCallbacks
     Provides detail on the available callbacks for the SSL Layer.
|oEnumerations and Typedefs
     Specifies the enums and Data Structures used by the SSL APIs.
|oFunctions
     Provides detail on the available APIs for the SSL Layer.
|\TLS Defines
oWLAN
|oCallbacks
     Provides detail on the available callbacks for the Wlan APIs.
|oDefines
     Specifies the macros and defines used by the Wlan APIs.
|oEnumerations and Typedefs
     Specifies the enums and Data Structures used by the Wlan APIs.
|\Functions
     Here are listed all the functions that implement the Wlan APIs.
oVersion
    Describes the APIs for reading the version information of the WINC firmware.
|oDefines
   Specifies the macros and defines used by the version APIs.
|\Functions
   Lists the APIs for reading the version information of the WINC firmware.
oSocketBSD compatible socket interface between the host layer and the network protocol stacks in the firmware
|oDefines
|oError CodesThe following list of macros are used to define the possible error codes
|oDataTypesSpecific Enumeration-typedefs used for socket operations
|oCallbacks
|oFunctions
|\Byte OrderThe following list of macros are used to convert between host representation and network byte order
oSpi Flash
|\Function
oSAM Port (PORT) DriverThis driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's General Purpose Input/Output (GPIO) pin functionality, for manual pin state reading and writing
oCompiler abstraction layer and code utilitiesCompiler abstraction layer and code utilities for Cortex-M0+ based Atmel SAM devices
|oStatus Codes
|oPreprocessor - Macro Recursion
|oPreprocessor - Macro Repeat
|oPreprocessor - Stringize
|\Preprocessor - Token Paste
oGlobal interrupt managementThis is a driver for global enabling and disabling of interrupts
|\Deprecated interrupt definitions
oAtmel part identification macrosThis collection of macros identify which series and families that the various Atmel parts belong to
|oAVR UC3 parts
|oAVR XMEGA parts
|omegaAVR parts
|\SAM parts
oSAM System Pin Multiplexer (SYSTEM PINMUX) DriverThis driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's physical I/O Pins, to alter the direction and input/drive characteristics as well as to configure the pin peripheral multiplexer selection
oSAM Serial Peripheral Interface (SERCOM SPI) DriverThis driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the SERCOM module in its SPI mode to transfer SPI data frames
oSAM System (SYSTEM) DriverThis driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's system relation functionality, necessary for the basic device operation
oSAM System Clock Management (SYSTEM CLOCK) DriverThis driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's clocking related functions
oSAM System Interrupt (SYSTEM INTERRUPT) DriverThis driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of internal software and hardware interrupts/exceptions
oBusy-Wait Delay RoutinesThis module provides simple loop-based delay routines for those applications requiring a brief wait during execution
oSAM External Interrupt (EXTINT) DriverThis driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of external interrupts generated by the physical device pins, including edge detection
oSerial Interface (Serial)See Quick start guide for Serial Interface service
oSAM Serial USART (SERCOM USART) DriverThis driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the SERCOM module in its USART mode to transfer or receive USART data frames
\Generic board supportThe generic board support module includes board-specific definitions and function prototypes, such as the board initialization function
 \SAM L21 Xplained Pro board