Lists the APIs for reading the version information of the WINC firmware.
Functions | |
NMI_API sint8 | m2m_ota_get_firmware_version (tstrM2mRev *pstrRev) |
Synchronous API to obtain the firmware version of the WINC image that is stored in the inactive flash partition. This is the image that would run on the WINC IC if m2m_ota_switch_firmware or m2m_ota_rollback were called, followed by a reset of the WINC IC. More... | |
sint8 | m2m_wifi_get_firmware_version (tstrM2mRev *pstrRev) |
Synchronous API to obtain the firmware version currently running on the WINC IC. More... | |
NMI_API sint8 m2m_ota_get_firmware_version | ( | tstrM2mRev * | pstrRev | ) |
Synchronous API to obtain the firmware version of the WINC image that is stored in the inactive flash partition. This is the image that would run on the WINC IC if m2m_ota_switch_firmware or m2m_ota_rollback were called, followed by a reset of the WINC IC.
Synchronous API to obtain the firmware version of the WINC image that is stored in the inactive flash partition. This is the image that would run on the WINC if m2m_ota_switch_firmware or m2m_ota_rollback were called, followed by a reset of the WINC.
[out] | pstrRev | pointer holds address of structure "tstrM2mRev" that contains the ota fw version parameters |
[out] | pstrRev | Pointer to variable of type tstrM2mRev which contains the ota fw version parameters. |
References hif_chip_sleep(), hif_chip_wake(), M2M_SUCCESS, and nm_get_ota_firmware_info().
Referenced by m2m_ota_rollback(), m2m_ota_switch_firmware(), and m2m_wifi_init_start().
sint8 m2m_wifi_get_firmware_version | ( | tstrM2mRev * | pstrRev | ) |
Synchronous API to obtain the firmware version currently running on the WINC IC.
Synchronous API to obtain the firmware version currently running on the WINC.
[out] | pstrRev | pointer holds address of structure "tstrM2mRev" that contains the firmware version parameters |
Get the Firmware version info from the active partition, as defined in the structure @ref tstrM2mRev.
[out] | pstrRev | Pointer to a variable of type tstrM2mRev, which contains the firmware version parameters. |
References hif_chip_sleep(), hif_chip_wake(), M2M_SUCCESS, and nm_get_firmware_full_info().
Referenced by m2m_wifi_init_start().