Functions | |
at_ble_status_t | at_ble_characteristic_value_get (at_ble_handle_t handle, uint8_t *value, uint16_t *actual_read_len) |
Reads a characteristic value. More... | |
at_ble_status_t | at_ble_characteristic_value_set (at_ble_handle_t handle, uint8_t *value, uint16_t len) |
Sets a characteristic value. More... | |
at_ble_status_t | at_ble_indication_send (at_ble_handle_t conn_handle, at_ble_handle_t attr_handle) |
Sends an Indication. More... | |
at_ble_status_t | at_ble_notification_send (at_ble_handle_t conn_handle, at_ble_handle_t attr_handle) |
Sends a Notification. More... | |
at_ble_status_t | at_ble_primary_service_define (at_ble_uuid_t *uuid, at_ble_handle_t *service_handle, at_ble_included_service_t *included_service_list, uint16_t included_service_count, at_ble_characteristic_t *characteristic_list, uint16_t characteristic_count) |
Defines a new Primary service along with its included services and characteristics. More... | |
at_ble_status_t | at_ble_read_authorize_reply (at_ble_handle_t conn_handle, at_ble_handle_t attr_handle, bool grant_authorization, bool update_value, uint8_t *value, uint16_t offset, uint16_t len) |
Replies to a read authorization request requested by by AT_BLE_READ_AUTHORIZE_REQUEST event. More... | |
at_ble_status_t | at_ble_secondary_service_define (at_ble_uuid_t *uuid, at_ble_handle_t *service_handle, at_ble_included_service_t *included_service_list, uint16_t included_service_count, at_ble_characteristic_t *characteristic_list, uint16_t characteristic_count) |
Defines a new Secondary service along with its included services and characteristics. More... | |
at_ble_status_t | at_ble_service_changed_notification_send (at_ble_handle_t conn_handle, at_ble_handle_t start_handle, at_ble_handle_t end_handle) |
Sends a Service changed Notification. More... | |
at_ble_status_t | at_ble_write_authorize_reply (at_ble_handle_t conn_handle, at_ble_handle_t attr_handle, bool grant_authorization) |
Replies to a write authorization request requested by by AT_BLE_WRITE_AUTHORIZE_REQUEST event. More... | |
at_ble_status_t at_ble_characteristic_value_get | ( | at_ble_handle_t | handle, |
uint8_t * | value, | ||
uint16_t * | actual_read_len | ||
) |
Reads a characteristic value.
[in] | handle | Characteristic value handle |
[out] | value | Read value will be returned here |
[in] | actual_read_len | Actual read length, in bytes |
References at_ble_att_error(), and gattm_att_get_value_req_handler().
Referenced by csc_serv_send_data().
at_ble_status_t at_ble_characteristic_value_set | ( | at_ble_handle_t | handle, |
uint8_t * | value, | ||
uint16_t | len | ||
) |
Sets a characteristic value.
[in] | handle | Characteristic value handle |
[in] | value | New value |
[in] | len | Value length, in bytes |
References at_ble_att_error(), and gattm_att_set_value_req_handler().
Referenced by csc_serv_send_data().
at_ble_status_t at_ble_indication_send | ( | at_ble_handle_t | conn_handle, |
at_ble_handle_t | attr_handle | ||
) |
Sends an Indication.
[in] | conn_handle | Handle of the connection to be notified |
[in] | attr_handle | Handle of the attribute originating the indication |
References GATTC_INDICATE, and gattc_send_evt_cmd_handler().
at_ble_status_t at_ble_notification_send | ( | at_ble_handle_t | conn_handle, |
at_ble_handle_t | attr_handle | ||
) |
Sends a Notification.
[in] | conn_handle | Handle of the connection to be notified |
[in] | attr_handle | Handle of the attribute originating the notification |
References GATTC_NOTIFY, and gattc_send_evt_cmd_handler().
Referenced by csc_serv_send_data().
at_ble_status_t at_ble_primary_service_define | ( | at_ble_uuid_t * | uuid, |
at_ble_handle_t * | service_handle, | ||
at_ble_included_service_t * | included_service_list, | ||
uint16_t | included_service_count, | ||
at_ble_characteristic_t * | characteristic_list, | ||
uint16_t | characteristic_count | ||
) |
Defines a new Primary service along with its included services and characteristics.
[in] | uuid | The primary service UUID |
[out] | service_handle | The Service handle will be returned here |
[in] | included_service_list | An array of included service references |
[in] | included_service_count | Number of elements in included_service_list |
[in,out] | characteristic_list | An array of characteristics included in the service, this array is update with respective characteristics handles. |
[in] | characteristic_count | Number of elements in charactristic_list |
References at_ble_service_define().
Referenced by csc_serv_init().
at_ble_status_t at_ble_read_authorize_reply | ( | at_ble_handle_t | conn_handle, |
at_ble_handle_t | attr_handle, | ||
bool | grant_authorization, | ||
bool | update_value, | ||
uint8_t * | value, | ||
uint16_t | offset, | ||
uint16_t | len | ||
) |
Replies to a read authorization request requested by by AT_BLE_READ_AUTHORIZE_REQUEST event.
[in] | conn_handle | Handle of the connection |
[in] | attr_handle | Handle of the attribute to read |
[in] | grant_authorization | If True, Authorization is granted |
[in] | update_value | If True, the value, offset, length of parameters will be used to update this attribute value |
[in] | value | New value |
[in] | offset | Where the writing starts |
[in] | len | Value length, in bytes |
at_ble_status_t at_ble_secondary_service_define | ( | at_ble_uuid_t * | uuid, |
at_ble_handle_t * | service_handle, | ||
at_ble_included_service_t * | included_service_list, | ||
uint16_t | included_service_count, | ||
at_ble_characteristic_t * | characteristic_list, | ||
uint16_t | characteristic_count | ||
) |
Defines a new Secondary service along with its included services and characteristics.
[in] | uuid | The secondary service UUID |
[out] | service_handle | The Service handle will be returned here |
[in] | included_service_list | An array of included service references |
[in] | included_service_count | Number of elements in included_service_list |
[in,out] | characteristic_list | An array of characteristics included in the service, this array is update with respective characteristics handles. |
[in] | characteristic_count | Number of elements in charactristic_list |
References at_ble_service_define().
at_ble_status_t at_ble_service_changed_notification_send | ( | at_ble_handle_t | conn_handle, |
at_ble_handle_t | start_handle, | ||
at_ble_handle_t | end_handle | ||
) |
Sends a Service changed Notification.
[in] | conn_handle | Handle of the connection to which the notification will be sent |
[in] | start_handle | Start of affected handle range |
[in] | end_handle | End of affected handle range |
References AT_BLE_INVALID_PARAM, and gattc_svc_changed_notification_cmd_handler().
at_ble_status_t at_ble_write_authorize_reply | ( | at_ble_handle_t | conn_handle, |
at_ble_handle_t | attr_handle, | ||
bool | grant_authorization | ||
) |
Replies to a write authorization request requested by by AT_BLE_WRITE_AUTHORIZE_REQUEST event.
[in] | conn_handle | Handle of the connection |
[in] | attr_handle | Handle of the attribute to write |
[in] | grant_authorization | If True, Authorization is granted |