![]() | |
![]() | Common standard I/O driver that implements the stdio read and write functions on AVR and SAM devices |
![]() ![]() | Common standard serial I/O management driver that implements a stdio serial interface on AVR and SAM devices |
![]() | |
![]() | |
![]() | |
![]() | |
![]() | |
![]() | |
![]() | |
![]() | |
![]() | Description of the BSP (<strong>B</strong>oard <strong>S</strong>upport <strong>P</strong>ackage) module. |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | Lists the available BSP (<strong>B</strong>oard <strong>S</strong>upport <strong>P</strong>ackage) APIs. |
![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | The WINC supports OTA (Over-The-Air) updates. |
![]() ![]() | Lists the different callbacks that can be used during OTA updates. |
![]() ![]() | Specifies the macros and defines used by the OTA APIs. |
![]() ![]() | Specifies the enums and Data Structures used by the OTA APIs. |
![]() ![]() | Lists the full set of available APIs to manage OTA updates and Host File Downloads. |
![]() | Provides a description of the SSL Layer. |
![]() ![]() | Provides detail on the available callbacks for the SSL Layer. |
![]() ![]() | Specifies the enums and Data Structures used by the SSL APIs. |
![]() ![]() | Provides detail on the available APIs for the SSL Layer. |
![]() ![]() | |
![]() ![]() ![]() | The following list of macros are used to define SSL Socket options |
![]() ![]() ![]() | The following list of macros defined the list of supported TLS Cipher suites |
![]() | Describes the APIs for reading the version information of the WINC firmware. |
![]() ![]() | Specifies the macros and defines used by the version APIs. |
![]() ![]() | Lists the APIs for reading the version information of the WINC firmware. |
![]() | |
![]() ![]() | Provides detail on the available callbacks for the Wlan APIs. |
![]() ![]() | Specifies the macros and defines used by the Wlan APIs. |
![]() ![]() | Specifies the enums and Data Structures used by the Wlan APIs. |
![]() ![]() | Here are listed all the functions that implement the Wlan APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Wlan Initialization APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Wlan Events APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Wifi Connection APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Wifi Scanning APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Wifi Hot-Spot (Access-Point) APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Bypass Mode APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Wifi Roaming APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Power-Save APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Wlan Configuration APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the System Time APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Wifi Provisioning APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Wifi Crypto APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the BLE APIs. |
![]() | BSD compatible socket interface between the host layer and the network protocol stacks in the firmware |
![]() ![]() | The following list of macros are used to define constants used throughout the socket layer, and SSL Socket options |
![]() ![]() ![]() | The following list of macros are used to define constants used throughout the socket layer |
![]() ![]() ![]() | |
![]() ![]() ![]() ![]() | The following list of macros are used to define SSL Socket options |
![]() ![]() ![]() ![]() | The following list of macros defined the list of supported TLS Cipher suites |
![]() ![]() | The following list of macros are used to convert between host representation and network byte order |
![]() ![]() | The following list of macros are used to define the possible error codes |
![]() ![]() | Specific Enumeration-typedefs used for socket operations |
![]() ![]() ![]() | Specific Enumeration used for asynchronous operations |
![]() ![]() | |
![]() ![]() | The function performs the necessary initializations for the socket library through the following steps: |
![]() | |
![]() ![]() | |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's General Purpose Input/Output (GPIO) pin functionality, for manual pin state reading and writing |
![]() | Compiler abstraction layer and code utilities for Cortex-M0+ based Atmel SAM devices |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | This is a driver for global enabling and disabling of interrupts |
![]() ![]() | |
![]() | This collection of macros identify which series and families that the various Atmel parts belong to |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's physical I/O Pins, to alter the direction and input/drive characteristics as well as to configure the pin peripheral multiplexer selection |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the SERCOM module in its SPI mode to transfer SPI data frames |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's system relation functionality, necessary for the basic device operation |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's clocking related functions |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of internal software and hardware interrupts/exceptions |
![]() | This module provides simple loop-based delay routines for those applications requiring a brief wait during execution |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of external interrupts generated by the physical device pins, including edge detection |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the TCC module within the device, for waveform generation and timing operations |
![]() | This module performs serial input/output functionalities via UART |
![]() | See Quick start guide for Serial Interface service |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the SERCOM module in its USART mode to transfer or receive USART data frames |
![]() | The generic board support module includes board-specific definitions and function prototypes, such as the board initialization function |
![]() ![]() | |
![]() ![]() ![]() | Symbols that describe features and capabilities of the board |