Data Structures | |
struct | _scanitem |
Store the scan list and then later populate when creating the database. More... | |
struct | at_ble_wifiprov_complete_ind |
struct | at_ble_wifiprov_scan_mode_change_ind_t |
struct | wifiprov_scanlist_ind |
Typedefs | |
typedef struct _scanitem | scanitem |
Store the scan list and then later populate when creating the database. More... | |
typedef struct _scanitem | scanitem |
Store the scan list and then later populate when creating the database. More... | |
Functions | |
void | wifiprov_complete_ind_handler (uint8_t *data, at_ble_wifiprov_complete_ind *param) |
Provisioning complete handler. More... | |
at_ble_status_t | wifiprov_configure_provisioning (uint8_t *localname, at_ble_auth_t lauthtype) |
Configure provisioning. More... | |
at_ble_status_t | wifiprov_create_db (void) |
Create provisioning database. More... | |
at_ble_status_t | wifiprov_disable (void) |
Disable provisioning. More... | |
at_ble_status_t | wifiprov_scan_list_ind_send (struct wifiprov_scanlist_ind *param) |
wifiprov_scan_list_ind_send More... | |
void | wifiprov_scan_mode_change_ind_handler (uint8_t *data, at_ble_wifiprov_scan_mode_change_ind_t *param) |
[Internal API] wifiprov_scan_mode_change_ind_handler More... | |
at_ble_status_t | wifiprov_scan_mode_change_ind_send (uint8_t scanmode) |
wifiprov_scan_mode_change_ind_send More... | |
at_ble_status_t | wifiprov_start (uint8_t *pin, uint8_t len) |
Start provisioning. More... | |
at_ble_status_t | wifiprov_wifi_con_update (uint8_t con_state) |
wifiprov_wifi_con_update More... | |
Store the scan list and then later populate when creating the database.
Store the scan list and then later populate when creating the database.
anonymous enum |
Messages from APP to WiFi Provisioning Profile.
anonymous enum |
WIFIPROV_SCANMODE.
When scan mode is used to send indication from App to the WiFi Prov profile, WIFIPROV_SCANMODE_SCANNING indicates Scanning is in progress WIFIPROV_SCANMODE_DONE indicates scanning is completed - note that this indication should only be used when no scan results were obtained during the scan These result in the database being updated When scan mode is used to send indication from WiFi Prov profile to the App, WIFIPROV_SCANMODE_SCANNING request to start WiFi scanning and supply scan results
Enumerator | |
---|---|
WIFIPROV_SCANMODE_INIT | |
WIFIPROV_SCANMODE_SCANNING |
Scanning is indicated as in progress. |
WIFIPROV_SCANMODE_DONE |
Scanning is indicated as complete. |
anonymous enum |
anonymous enum |
Messages from APP to WiFi Provisioning Profile.
anonymous enum |
WIFIPROV_SCANMODE.
When scan mode is used to send indication from App to the WiFi Prov profile, WIFIPROV_SCANMODE_SCANNING indicates Scanning is in progress WIFIPROV_SCANMODE_DONE indicates scanning is completed - note that this indication should only be used when no scan results were obtained during the scan These result in the database being updated When scan mode is used to send indication from WiFi Prov profile to the App, WIFIPROV_SCANMODE_SCANNING request to start WiFi scanning and supply scan results
Enumerator | |
---|---|
WIFIPROV_SCANMODE_INIT | |
WIFIPROV_SCANMODE_SCANNING |
Scanning is indicated as in progress. |
WIFIPROV_SCANMODE_DONE |
Scanning is indicated as complete. |
anonymous enum |
void wifiprov_complete_ind_handler | ( | uint8_t * | data, |
at_ble_wifiprov_complete_ind * | param | ||
) |
Provisioning complete handler.
Provisioning complete handler.
[in] | data | |
[in] | param |
References INTERFACE_UNPACK_BLOCK, INTERFACE_UNPACK_DONE, INTERFACE_UNPACK_INIT, INTERFACE_UNPACK_UINT8, MAX_WIPROVTASK_PASS_LENGTH, MAX_WIPROVTASK_SSID_LENGTH, at_ble_wifiprov_complete_ind::passphrase, at_ble_wifiprov_complete_ind::passphrase_length, at_ble_wifiprov_complete_ind::sec_type, at_ble_wifiprov_complete_ind::ssid, at_ble_wifiprov_complete_ind::ssid_length, and at_ble_wifiprov_complete_ind::status.
Referenced by handle_ble_event().
at_ble_status_t wifiprov_configure_provisioning | ( | uint8_t * | localname, |
at_ble_auth_t | lauthtype | ||
) |
Configure provisioning.
[in] | localname | must be a null terminated string |
[in] | lauthtype | auth type to be used for provisioning |
[in] | localname | must be a null terminated string |
References AT_BLE_FAILURE, INTERFACE_MSG_DONE, INTERFACE_MSG_INIT, INTERFACE_PACK_ARG_BLOCK, INTERFACE_PACK_ARG_UINT8, INTERFACE_SEND_WAIT, INTERFACE_UNPACK_UINT8, MAX_LOCALNAME_LENGTH, TASK_WIFIPROV, WIFIPROV_CONFIGURE_CFM, and WIFIPROV_CONFIGURE_REQ.
Referenced by ble_prov_init().
at_ble_status_t wifiprov_create_db | ( | void | ) |
Create provisioning database.
References AT_BLE_FAILURE, INTERFACE_MSG_DONE, INTERFACE_MSG_INIT, INTERFACE_PACK_ARG_UINT8, INTERFACE_SEND_WAIT, INTERFACE_UNPACK_UINT8, TASK_WIFIPROV, WIFIPROV_CREATE_DB_CFM, and WIFIPROV_CREATE_DB_REQ.
Referenced by ble_prov_init().
at_ble_status_t wifiprov_disable | ( | void | ) |
Disable provisioning.
If connected, disconnect, if advertising stop advertising.
References INTERFACE_MSG_DONE, INTERFACE_MSG_INIT, INTERFACE_SEND_NO_WAIT, TASK_WIFIPROV, and WIFIPROV_DISABLE_CMD.
Referenced by ble_prov_stop().
at_ble_status_t wifiprov_scan_list_ind_send | ( | struct wifiprov_scanlist_ind * | param | ) |
wifiprov_scan_list_ind_send
[in] | param |
References INTERFACE_MSG_DONE, INTERFACE_MSG_INIT, INTERFACE_PACK_ARG_BLOCK, INTERFACE_SEND_NO_WAIT, TASK_WIFIPROV, and WIFIPROV_SCANLIST_IND.
Referenced by ble_prov_scan_result().
void wifiprov_scan_mode_change_ind_handler | ( | uint8_t * | data, |
at_ble_wifiprov_scan_mode_change_ind_t * | param | ||
) |
[Internal API] wifiprov_scan_mode_change_ind_handler
Scan mode has changed notification
[in] | data | |
[in] | param | WIFIPROV_SCANMODE_SCANNING WIFIPROV_SCANMODE_DONE |
References INTERFACE_UNPACK_DONE, INTERFACE_UNPACK_INIT, INTERFACE_UNPACK_UINT8, and at_ble_wifiprov_scan_mode_change_ind_t::scanmode.
Referenced by handle_ble_event().
at_ble_status_t wifiprov_scan_mode_change_ind_send | ( | uint8_t | scanmode | ) |
wifiprov_scan_mode_change_ind_send
[in] | scanmode |
References INTERFACE_MSG_DONE, INTERFACE_MSG_INIT, INTERFACE_PACK_ARG_UINT8, INTERFACE_SEND_NO_WAIT, TASK_WIFIPROV, and WIFIPROV_SCAN_MODE_CHANGE_IND.
Referenced by ble_prov_process_event().
at_ble_status_t wifiprov_start | ( | uint8_t * | pin, |
uint8_t | len | ||
) |
Start provisioning.
If idle then start
[in] | pin | 6 digit decimal PIN |
[in] | len |
References INTERFACE_MSG_DONE, INTERFACE_MSG_INIT, INTERFACE_PACK_ARG_BLOCK, INTERFACE_SEND_NO_WAIT, TASK_WIFIPROV, and WIFIPROV_START_CMD.
Referenced by ble_prov_start().
at_ble_status_t wifiprov_wifi_con_update | ( | uint8_t | con_state | ) |
wifiprov_wifi_con_update
wifiprov_wifi_con_update.
[in] | con_state |
References INTERFACE_MSG_DONE, INTERFACE_MSG_INIT, INTERFACE_PACK_ARG_UINT8, INTERFACE_SEND_NO_WAIT, TASK_WIFIPROV, and WIFIPROV_CONNECTION_STATE_CHANGE_IND.