![]() | |
![]() | |
![]() | |
![]() | See Quickstart guide for SAM SPI driver |
![]() | The Universal Asynchronous Receiver Transmitter features a two-pin UART that can be used for communication and trace purposes and offers an ideal medium for in-situ programming solutions |
![]() | Receiver Transmitter (USART) |
![]() | Common standard I/O driver that implements the stdio read and write functions on AVR and SAM devices |
![]() ![]() | Common standard serial I/O management driver that implements a stdio serial interface on AVR and SAM devices |
![]() | |
![]() ![]() | |
![]() | |
![]() | |
![]() | |
![]() | |
![]() | |
![]() | |
![]() | |
![]() | |
![]() | Description of the BSP (<strong>B</strong>oard <strong>S</strong>upport <strong>P</strong>ackage) module. |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | Lists the available BSP (<strong>B</strong>oard <strong>S</strong>upport <strong>P</strong>ackage) APIs. |
![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | The WINC supports OTA (Over-The-Air) updates. |
![]() ![]() | Lists the different callbacks that can be used during OTA updates. |
![]() ![]() | Specifies the macros and defines used by the OTA APIs. |
![]() ![]() | Specifies the enums and Data Structures used by the OTA APIs. |
![]() ![]() | Lists the full set of available APIs to manage OTA updates and Host File Downloads. |
![]() | Provides a description of the SSL Layer. |
![]() ![]() | Provides detail on the available callbacks for the SSL Layer. |
![]() ![]() | Specifies the enums and Data Structures used by the SSL APIs. |
![]() ![]() | Provides detail on the available APIs for the SSL Layer. |
![]() ![]() | |
![]() ![]() ![]() | The following list of macros are used to define SSL Socket options |
![]() ![]() ![]() | The following list of macros defined the list of supported TLS Cipher suites |
![]() | Describes the APIs for reading the version information of the WINC firmware. |
![]() ![]() | Specifies the macros and defines used by the version APIs. |
![]() ![]() | Lists the APIs for reading the version information of the WINC firmware. |
![]() | |
![]() ![]() | Provides detail on the available callbacks for the Wlan APIs. |
![]() ![]() | Specifies the macros and defines used by the Wlan APIs. |
![]() ![]() | Specifies the enums and Data Structures used by the Wlan APIs. |
![]() ![]() | Here are listed all the functions that implement the Wlan APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Wlan Initialization APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Wlan Events APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Wifi Connection APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Wifi Scanning APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Wifi Hot-Spot (Access-Point) APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Bypass Mode APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Wifi Roaming APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Power-Save APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Wlan Configuration APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the System Time APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Wifi Provisioning APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the Wifi Crypto APIs. |
![]() ![]() ![]() | Here are listed all the functions that implement the BLE APIs. |
![]() | BSD compatible socket interface between the host layer and the network protocol stacks in the firmware |
![]() ![]() | The following list of macros are used to define constants used throughout the socket layer, and SSL Socket options |
![]() ![]() ![]() | The following list of macros are used to define constants used throughout the socket layer |
![]() ![]() ![]() | |
![]() ![]() ![]() ![]() | The following list of macros are used to define SSL Socket options |
![]() ![]() ![]() ![]() | The following list of macros defined the list of supported TLS Cipher suites |
![]() ![]() | The following list of macros are used to convert between host representation and network byte order |
![]() ![]() | The following list of macros are used to define the possible error codes |
![]() ![]() | Specific Enumeration-typedefs used for socket operations |
![]() ![]() ![]() | Specific Enumeration used for asynchronous operations |
![]() ![]() | |
![]() ![]() | The function performs the necessary initializations for the socket library through the following steps: |
![]() | |
![]() ![]() | |
![]() | This is a stub on the SAM Power Manager Control (PMC) for the sleepmgr service |
![]() | Compiler abstraction layer and code utilities for AT91SAM |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | This is a driver for global enabling and disabling of interrupts |
![]() ![]() | |
![]() | This collection of macros identify which series and families that the various Atmel parts belong to |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | |
![]() ![]() | Generic clocks are configurable clocks which run outside the system clock domain |
![]() ![]() | This group contains functions and definitions related to configuring and enabling/disabling on-chip oscillators |
![]() ![]() | This group contains functions and definitions related to configuring and enabling/disabling on-chip PLLs |
![]() ![]() | See Quick Start Guide for the System Clock Management |
![]() | See Quick start guide for the common IOPORT service |
![]() | This module provides simple loop-based delay routines for those applications requiring a brief wait during execution |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Timer Counter functionality |
![]() | See Quick start guide for Serial Interface service |
![]() | Transmitter (USART) |
![]() | The generic board support module includes board-specific definitions and function prototypes, such as the board initialization function |
![]() | This is the common API for GPIO |