Message structure used to inform APP that an error has occurred in the profile server role task.
#include <profiles.h>
Data Fields | |
uint16_t | conhdl |
Connection Handle. More... | |
uint16_t | msg_id |
Message ID. More... | |
uint8_t | status |
Status. More... | |
uint16_t prf_server_error_ind::conhdl |
Connection Handle.
uint16_t prf_server_error_ind::msg_id |
Message ID.
uint8_t prf_server_error_ind::status |
Status.