This driver for Atmel® | SMART SAM XDMA Controller (XDMAC) is a AHB-protocol central direct memory access controller.
It performs peripheral data transfer and memory move operations over one or two bus ports through the unidirectional communication channel. This is a driver for the configuration, enabling, disabling, and use of the XDMAC peripheral.
Devices from the following series can use this module:
The outline of this documentation is as follows:
There are no prerequisites for this module.
The DMA Controller (XDMAC) is a AHB-protocol central direct memory access controller. It performs peripheral data transfer and memory move operations over one or two bus ports through the unidirectional communication channel. Each channel is fully programmable and provides both peripheral or memory to memory transfer. The channel features are configurable at implementation time.
There are no special considerations for this module.
For extra information, see Extra Information for Extensible Direct Memory Access Controller Driver. This includes:
For a list of examples related to this driver, see Examples for Direct Memory Access Controller Driver.
Data Structures | |
struct | lld_view0 |
Structure for storing parameters for DMA view0 that can be performed by the DMA Master transfer. More... | |
struct | lld_view1 |
Structure for storing parameters for DMA view1 that can be performed by the DMA Master transfer. More... | |
struct | lld_view2 |
Structure for storing parameters for DMA view2 that can be performed by the DMA Master transfer. More... | |
struct | lld_view3 |
Structure for storing parameters for DMA view3 that can be performed by the DMA Master transfer. More... | |
struct | xdmac_channel_config_t |
XDMA config register for channel. More... | |
Functions | |
static void | xdmac_channel_disable (Xdmac *xdmac, uint32_t channel_num) |
Disables the relevant channel of given XDMAC. More... | |
static void | xdmac_channel_disable_interrupt (Xdmac *xdmac, uint32_t channel_num, uint32_t mask) |
Disable interrupt with mask on the relevant channel of given XDMA. More... | |
static void | xdmac_channel_enable (Xdmac *xdmac, uint32_t channel_num) |
enables the relevant channel of given XDMAC. More... | |
static void | xdmac_channel_enable_interrupt (Xdmac *xdmac, uint32_t channel_num, uint32_t mask) |
Enable interrupt with mask on the relevant channel of given XDMA. More... | |
static uint32_t | xdmac_channel_get_interrupt_mask (Xdmac *xdmac, uint32_t channel_num) |
Get interrupt mask for the relevant channel of given XDMA. More... | |
static uint32_t | xdmac_channel_get_interrupt_status (Xdmac *xdmac, uint32_t channel_num) |
Get interrupt status for the relevant channel of given XDMA. More... | |
static uint32_t | xdmac_channel_get_status (Xdmac *xdmac) |
Get Global channel status of given XDMAC. More... | |
static void | xdmac_channel_read_suspend (Xdmac *xdmac, uint32_t channel_num) |
Suspend the relevant channel's read. More... | |
static void | xdmac_channel_readwrite_resume (Xdmac *xdmac, uint32_t channel_num) |
Resume the relevant channel's read & write. More... | |
static void | xdmac_channel_readwrite_suspend (Xdmac *xdmac, uint32_t channel_num) |
Suspend the relevant channel's read & write. More... | |
static void | xdmac_channel_set_block_control (Xdmac *xdmac, uint32_t channel_num, uint32_t blen) |
Set block length for the relevant channel of given XDMA. More... | |
static void | xdmac_channel_set_config (Xdmac *xdmac, uint32_t channel_num, uint32_t config) |
Set configuration for the relevant channel of given XDMA. More... | |
static void | xdmac_channel_set_datastride_mempattern (Xdmac *xdmac, uint32_t channel_num, uint32_t dds_msp) |
Set the relevant channel's data stride memory pattern of given XDMA. More... | |
static void | xdmac_channel_set_descriptor_addr (Xdmac *xdmac, uint32_t channel_num, uint32_t desc_addr, uint8_t ndaif) |
Set next descriptor's address & interface for the relevant channel of given XDMA. More... | |
static void | xdmac_channel_set_descriptor_control (Xdmac *xdmac, uint32_t channel_num, uint32_t config) |
Set next descriptor's configuration for the relevant channel of given XDMA. More... | |
static void | xdmac_channel_set_destination_addr (Xdmac *xdmac, uint32_t channel_num, uint32_t dst_addr) |
Set destination address for the relevant channel of given XDMA. More... | |
static void | xdmac_channel_set_destination_microblock_stride (Xdmac *xdmac, uint32_t channel_num, uint32_t dubs) |
Set the relevant channel's destination microblock stride of given XDMA. More... | |
static void | xdmac_channel_set_microblock_control (Xdmac *xdmac, uint32_t channel_num, uint32_t ublen) |
Set microblock length for the relevant channel of given XDMA. More... | |
static void | xdmac_channel_set_source_addr (Xdmac *xdmac, uint32_t channel_num, uint32_t src_addr) |
Set source address for the relevant channel of given XDMA. More... | |
static void | xdmac_channel_set_source_microblock_stride (Xdmac *xdmac, uint32_t channel_num, uint32_t subs) |
Set the relevant channel's source microblock stride of given XDMA. More... | |
static void | xdmac_channel_software_flush_request (Xdmac *xdmac, uint32_t channel_num) |
Set software flush request on the relevant channel. More... | |
static void | xdmac_channel_software_request (Xdmac *xdmac, uint32_t channel_num) |
Set software transfer request on the relevant channel. More... | |
static void | xdmac_channel_write_suspend (Xdmac *xdmac, uint32_t channel_num) |
Suspend the relevant channel's write. More... | |
void | xdmac_configure_transfer (Xdmac *xdmac, uint32_t channel_num, xdmac_channel_config_t *p_cfg) |
Configure DMA for a transfer. More... | |
static void | xdmac_disable_interrupt (Xdmac *xdmac, uint32_t channel_num) |
Disables XDMAC global interrupt. More... | |
static void | xdmac_enable_interrupt (Xdmac *xdmac, uint32_t channel_num) |
Enables XDMAC global interrupt. More... | |
static uint32_t | xdmac_get_arbiter (Xdmac *xdmac) |
Get XDMAC global weighted arbiter configuration. More... | |
static uint32_t | xdmac_get_config (Xdmac *xdmac) |
Get XDMAC global configuration. More... | |
static uint32_t | xdmac_get_interrupt_mask (Xdmac *xdmac) |
Get XDMAC global interrupt mask. More... | |
static uint32_t | xdmac_get_interrupt_status (Xdmac *xdmac) |
Get XDMAC global interrupt status. More... | |
static uint32_t | xdmac_get_software_request_status (Xdmac *xdmac) |
Get software transfer status of the relevant channel. More... | |
static uint32_t | xdmac_get_type (Xdmac *xdmac) |
Get XDMAC global type. More... | |
#define XDMAC_CHANNEL_HWID_AES_RX 38 |
#define XDMAC_CHANNEL_HWID_AES_TX 37 |
#define XDMAC_CHANNEL_HWID_AFEC0 35 |
#define XDMAC_CHANNEL_HWID_AFEC1 36 |
#define XDMAC_CHANNEL_HWID_DAC 30 |
#define XDMAC_CHANNEL_HWID_HSMCI 0 |
DMA channel hardware interface number.
#define XDMAC_CHANNEL_HWID_PIOA 34 |
#define XDMAC_CHANNEL_HWID_PWM0 13 |
#define XDMAC_CHANNEL_HWID_PWM1 39 |
#define XDMAC_CHANNEL_HWID_QSPI_RX 6 |
#define XDMAC_CHANNEL_HWID_QSPI_TX 5 |
#define XDMAC_CHANNEL_HWID_SPI0_RX 2 |
#define XDMAC_CHANNEL_HWID_SPI0_TX 1 |
#define XDMAC_CHANNEL_HWID_SPI1_RX 4 |
#define XDMAC_CHANNEL_HWID_SPI1_TX 3 |
#define XDMAC_CHANNEL_HWID_SSC_RX 33 |
#define XDMAC_CHANNEL_HWID_SSC_TX 32 |
#define XDMAC_CHANNEL_HWID_TC0 40 |
#define XDMAC_CHANNEL_HWID_TC1 41 |
#define XDMAC_CHANNEL_HWID_TC2 42 |
#define XDMAC_CHANNEL_HWID_TC3 43 |
#define XDMAC_CHANNEL_HWID_TWIHS0_RX 15 |
#define XDMAC_CHANNEL_HWID_TWIHS0_TX 14 |
#define XDMAC_CHANNEL_HWID_TWIHS1_RX 17 |
#define XDMAC_CHANNEL_HWID_TWIHS1_TX 16 |
#define XDMAC_CHANNEL_HWID_TWIHS2_RX 19 |
#define XDMAC_CHANNEL_HWID_TWIHS2_TX 18 |
#define XDMAC_CHANNEL_HWID_UART0_RX 21 |
#define XDMAC_CHANNEL_HWID_UART0_TX 20 |
#define XDMAC_CHANNEL_HWID_UART1_RX 23 |
#define XDMAC_CHANNEL_HWID_UART1_TX 22 |
#define XDMAC_CHANNEL_HWID_UART2_RX 25 |
#define XDMAC_CHANNEL_HWID_UART2_TX 24 |
#define XDMAC_CHANNEL_HWID_UART3_RX 27 |
#define XDMAC_CHANNEL_HWID_UART3_TX 26 |
#define XDMAC_CHANNEL_HWID_UART4_RX 29 |
#define XDMAC_CHANNEL_HWID_UART4_TX 28 |
#define XDMAC_CHANNEL_HWID_USART0_RX 8 |
#define XDMAC_CHANNEL_HWID_USART0_TX 7 |
#define XDMAC_CHANNEL_HWID_USART1_RX 10 |
#define XDMAC_CHANNEL_HWID_USART1_TX 9 |
#define XDMAC_CHANNEL_HWID_USART2_RX 12 |
#define XDMAC_CHANNEL_HWID_USART2_TX 11 |
#define XDMAC_UBC_NDE (0x1u << 24) |
#define XDMAC_UBC_NDE_FETCH_DIS (0x0u << 24) |
#define XDMAC_UBC_NDE_FETCH_EN (0x1u << 24) |
#define XDMAC_UBC_NDEN (0x1u << 26) |
#define XDMAC_UBC_NDEN_UNCHANGED (0x0u << 26) |
#define XDMAC_UBC_NDEN_UPDATED (0x1u << 26) |
#define XDMAC_UBC_NSEN (0x1u << 25) |
#define XDMAC_UBC_NSEN_UNCHANGED (0x0u << 25) |
#define XDMAC_UBC_NSEN_UPDATED (0x1u << 25) |
#define XDMAC_UBC_NVIEW_Msk (0x3u << XDMAC_UBC_NVIEW_Pos) |
#define XDMAC_UBC_NVIEW_NDV0 (0x0u << XDMAC_UBC_NVIEW_Pos) |
#define XDMAC_UBC_NVIEW_NDV1 (0x1u << XDMAC_UBC_NVIEW_Pos) |
#define XDMAC_UBC_NVIEW_NDV2 (0x2u << XDMAC_UBC_NVIEW_Pos) |
#define XDMAC_UBC_NVIEW_NDV3 (0x3u << XDMAC_UBC_NVIEW_Pos) |
#define XDMAC_UBC_NVIEW_Pos 27 |
#define XDMAC_UBC_UBLEN | ( | value | ) | ((XDMAC_UBC_UBLEN_Msk & ((value) << XDMAC_UBC_UBLEN_Pos))) |
#define XDMAC_UBC_UBLEN_Msk (0xffffffu << XDMAC_UBC_UBLEN_Pos) |
#define XDMAC_UBC_UBLEN_Pos 0 |
|
inlinestatic |
Disables the relevant channel of given XDMAC.
[out] | xdmac | Module hardware register base address pointer. |
[in] | channel_num | XDMA Channel number (range 0 to 23) |
References Assert.
Referenced by XDMAC_Handler().
|
inlinestatic |
Disable interrupt with mask on the relevant channel of given XDMA.
[out] | xdmac | Module hardware register base address pointer. |
[in] | channel_num | XDMA Channel number (range 0 to 23). |
[in] | mask | Interrupt mask. |
References Assert.
|
inlinestatic |
enables the relevant channel of given XDMAC.
[out] | xdmac | Module hardware register base address pointer. |
[in] | channel_num | XDMA Channel number (range 0 to 23) |
References Assert.
Referenced by spi_xdmac_configure().
|
inlinestatic |
Enable interrupt with mask on the relevant channel of given XDMA.
[out] | xdmac | Module hardware register base address pointer. |
[in] | channel_num | XDMA Channel number (range 0 to 23). |
[in] | mask | Interrupt mask. |
References Assert.
Referenced by spi_xdmac_init().
|
inlinestatic |
Get interrupt mask for the relevant channel of given XDMA.
[out] | xdmac | Module hardware register base address pointer. |
[in] | channel_num | XDMA Channel number (range 0 to 23). |
References Assert.
|
inlinestatic |
Get interrupt status for the relevant channel of given XDMA.
[out] | xdmac | Module hardware register base address pointer. |
[in] | channel_num | XDMA Channel number (range 0 to 23). |
References Assert.
Referenced by xdmac_channel_software_flush_request(), xdmac_configure_transfer(), and XDMAC_Handler().
|
inlinestatic |
Get Global channel status of given XDMAC.
[out] | xdmac | Module hardware register base address pointer. |
References Assert.
|
inlinestatic |
Suspend the relevant channel's read.
[out] | xdmac | Module hardware register base address pointer. |
[in] | channel_num | XDMA Channel number (range 0 to 23). |
References Assert.
|
inlinestatic |
Resume the relevant channel's read & write.
[out] | xdmac | Module hardware register base address pointer. |
[in] | channel_num | XDMA Channel number (range 0 to 23). |
References Assert.
|
inlinestatic |
Suspend the relevant channel's read & write.
[out] | xdmac | Module hardware register base address pointer. |
[in] | channel_num | XDMA Channel number (range 0 to 23). |
References Assert.
|
inlinestatic |
Set block length for the relevant channel of given XDMA.
[out] | xdmac | Module hardware register base address pointer |
[in] | channel_num | XDMA Channel number (range 0 to 23) |
[in] | blen | Block length. |
References Assert.
Referenced by xdmac_configure_transfer().
|
inlinestatic |
Set configuration for the relevant channel of given XDMA.
[out] | xdmac | Module hardware register base address pointer |
[in] | channel_num | XDMA Channel number (range 0 to 23) |
[in] | config | Channel configuration. |
References Assert.
Referenced by xdmac_configure_transfer().
|
inlinestatic |
Set the relevant channel's data stride memory pattern of given XDMA.
[out] | xdmac | Module hardware register base address pointer |
[in] | channel_num | XDMA Channel number (range 0 to 23) |
[in] | dds_msp | Data stride memory pattern. |
References Assert.
Referenced by xdmac_configure_transfer().
|
inlinestatic |
Set next descriptor's address & interface for the relevant channel of given XDMA.
[out] | xdmac | Module hardware register base address pointer |
[in] | channel_num | DMA Channel number (range 0 to 23) |
[in] | desc_addr | Address of next descriptor. |
[in] | ndaif | Interface of next descriptor. |
References Assert.
|
inlinestatic |
Set next descriptor's configuration for the relevant channel of given XDMA.
[out] | xdmac | Module hardware register base address pointer |
[in] | channel_num | DMA Channel number (range 0 to 23) |
[in] | config | Configuration of next descriptor. |
References Assert.
Referenced by spi_xdmac_init().
|
inlinestatic |
Set destination address for the relevant channel of given XDMA.
[out] | xdmac | Module hardware register base address pointer |
[in] | channel_num | DMA Channel number (range 0 to 23) |
[in] | dst_addr | Destination address |
References Assert.
Referenced by xdmac_configure_transfer().
|
inlinestatic |
Set the relevant channel's destination microblock stride of given XDMA.
[out] | xdmac | Module hardware register base address pointer |
[in] | channel_num | XDMA Channel number (range 0 to 23) |
[in] | dubs | Destination microblock stride. |
References Assert.
Referenced by xdmac_configure_transfer().
|
inlinestatic |
Set microblock length for the relevant channel of given XDMA.
[out] | xdmac | Module hardware register base address pointer |
[in] | channel_num | DMA Channel number (range 0 to 23) |
[in] | ublen | Microblock length. |
References Assert.
Referenced by xdmac_configure_transfer().
|
inlinestatic |
Set source address for the relevant channel of given XDMA.
[out] | xdmac | Module hardware register base address pointer |
[in] | channel_num | DMA Channel number (range 0 to 23) |
[in] | src_addr | Source address |
References Assert.
Referenced by xdmac_configure_transfer().
|
inlinestatic |
Set the relevant channel's source microblock stride of given XDMA.
[out] | xdmac | Module hardware register base address pointer |
[in] | channel_num | XDMA Channel number (range 0 to 23) |
[in] | subs | Source microblock stride. |
References Assert.
Referenced by xdmac_configure_transfer().
|
inlinestatic |
Set software flush request on the relevant channel.
[out] | xdmac | Module hardware register base address pointer. |
[in] | channel_num | XDMA Channel number (range 0 to 23). |
References Assert, and xdmac_channel_get_interrupt_status().
|
inlinestatic |
Set software transfer request on the relevant channel.
[out] | xdmac | Module hardware register base address pointer. |
[in] | channel_num | XDMA Channel number (range 0 to 23). |
References Assert.
|
inlinestatic |
Suspend the relevant channel's write.
[out] | xdmac | Module hardware register base address pointer. |
[in] | channel_num | XDMA Channel number (range 0 to 23). |
References Assert.
void xdmac_configure_transfer | ( | Xdmac * | xdmac, |
uint32_t | channel_num, | ||
xdmac_channel_config_t * | cfg | ||
) |
Configure DMA for a transfer.
[out] | xdmac | Module hardware register base address pointer. |
[in] | channel_num | The used channel number. |
[in] | cfg | The configuration for used channel |
References Assert, xdmac_channel_config_t::mbr_bc, xdmac_channel_config_t::mbr_cfg, xdmac_channel_config_t::mbr_da, xdmac_channel_config_t::mbr_ds, xdmac_channel_config_t::mbr_dus, xdmac_channel_config_t::mbr_sa, xdmac_channel_config_t::mbr_sus, xdmac_channel_config_t::mbr_ubc, xdmac_channel_get_interrupt_status(), xdmac_channel_set_block_control(), xdmac_channel_set_config(), xdmac_channel_set_datastride_mempattern(), xdmac_channel_set_destination_addr(), xdmac_channel_set_destination_microblock_stride(), xdmac_channel_set_microblock_control(), xdmac_channel_set_source_addr(), and xdmac_channel_set_source_microblock_stride().
Referenced by spi_xdmac_configure().
|
inlinestatic |
Disables XDMAC global interrupt.
[out] | xdmac | Module hardware register base address pointer. |
[in] | channel_num | XDMA Channel number (range 0 to 23). |
References Assert.
|
inlinestatic |
Enables XDMAC global interrupt.
[out] | xdmac | Module hardware register base address pointer. |
[in] | channel_num | XDMA Channel number (range 0 to 23). |
References Assert.
Referenced by spi_xdmac_init().
|
inlinestatic |
Get XDMAC global weighted arbiter configuration.
[out] | xdmac | Module hardware register base address pointer. |
References Assert.
|
inlinestatic |
Get XDMAC global configuration.
[out] | xdmac | Module hardware register base address pointer. |
References Assert.
|
inlinestatic |
Get XDMAC global interrupt mask.
[out] | xdmac | Module hardware register base address pointer. |
References Assert.
|
inlinestatic |
Get XDMAC global interrupt status.
[out] | xdmac | Module hardware register base address pointer. |
References Assert.
|
inlinestatic |
Get software transfer status of the relevant channel.
[out] | xdmac | Module hardware register base address pointer. |
References Assert.
|
inlinestatic |
Get XDMAC global type.
[out] | xdmac | Module hardware register base address pointer. |
References Assert.