Microchip® Advanced Software Framework

Structure for storing parameters for DMA view3 that can be performed by the DMA Master transfer.

#include <xdmac.h>

Data Fields

uint32_t mbr_bc
 Block Control Member. More...
 
uint32_t mbr_cfg
 Configuration Register. More...
 
uint32_t mbr_da
 Destination Address Member. More...
 
uint32_t mbr_ds
 Data Stride Member. More...
 
uint32_t mbr_dus
 Destination Microblock Stride Member. More...
 
uint32_t mbr_nda
 Next Descriptor Address number. More...
 
uint32_t mbr_sa
 Source Address Member. More...
 
uint32_t mbr_sus
 Source Microblock Stride Member. More...
 
uint32_t mbr_ubc
 Microblock Control Member. More...
 

uint32_t lld_view3::mbr_bc

Block Control Member.

uint32_t lld_view3::mbr_cfg

Configuration Register.

uint32_t lld_view3::mbr_da

Destination Address Member.

uint32_t lld_view3::mbr_ds

Data Stride Member.

uint32_t lld_view3::mbr_dus

Destination Microblock Stride Member.

uint32_t lld_view3::mbr_nda

Next Descriptor Address number.

uint32_t lld_view3::mbr_sa

Source Address Member.

uint32_t lld_view3::mbr_sus

Source Microblock Stride Member.

uint32_t lld_view3::mbr_ubc

Microblock Control Member.