Here are listed all the functions that implement the Power-Save APIs.
Functions | |
uint8 | m2m_wifi_get_sleep_mode (void) |
Get the current Power save mode. More... | |
sint8 | m2m_wifi_request_sleep (uint32 u32SlpReqTime) |
Asynchronous API to place the WINC into sleep mode for a specified period of time. More... | |
sint8 | m2m_wifi_set_lsn_int (tstrM2mLsnInt *pstrM2mLsnInt) |
Set the Wi-Fi listen interval for power save operation. It is represented in units of AP Beacon periods. More... | |
sint8 | m2m_wifi_set_power_profile (uint8 u8PwrMode) |
Change the power profile mode Not implemented in WINC3400 firmware. More... | |
sint8 | m2m_wifi_set_sleep_mode (uint8 PsTyp, uint8 BcastEn) |
Set the power saving mode for the WINC3400. More... | |
Get the current Power save mode.
Synchronous API to retrieve the current power save mode of the WINC.
References hif_get_sleep_mode().
Referenced by os_m2m_wifi_get_sleep_mode().
Asynchronous API to place the WINC into sleep mode for a specified period of time.
Power-save sleep request function, which requests the WINC device to sleep in the currently configured power save mode, as set using @ref m2m_wifi_set_sleep_mode, for a specific time as defined by the parameter u32SlpReqTime (measured in milliseconds). This function should be used when the WINC is running in @ref M2M_PS_MANUAL power save mode only. A wake up request is automatically performed by the WINC device when any host driver API function, e.g. Wi-Fi or socket operation is called.
[in] | u32SlpReqTime | Request sleep time in ms. The best recommended sleep duration is left to be determined by the application. Taking into account that if the application sends notifications very rarely, sleeping for a long time can be a power-efficient decision. In contrast, applications that are sensitive for long periods of absence can experience performance degradation in the connection if long sleeping times are used. |
References hif_get_sleep_mode(), hif_send(), M2M_PS_MANUAL, M2M_REQ_GROUP_WIFI, M2M_SUCCESS, M2M_WIFI_REQ_DOZE, NULL, and tstrM2mSlpReqTime::u32SleepTime.
Referenced by os_m2m_wifi_request_sleep_imp().
NMI_API sint8 m2m_wifi_set_lsn_int | ( | tstrM2mLsnInt * | pstrM2mLsnInt | ) |
Set the Wi-Fi listen interval for power save operation. It is represented in units of AP Beacon periods.
Asynchronous API to set Wi-Fi listen interval for power save operation.
[in] | pstrM2mLsnInt | Structure holding the listen interval configurations. |
This is one of the two synchronous power-save setting functions that allow the host MCU application to tweak the system power consumption. Such tweaking can be done by modifying the Wi-Fi listen interval. The listen interval is how many beacon periods the station can sleep before it wakes up to receive data buffered in the AP. It is represented in units of AP beacon periods(100ms).
[in] | pstrM2mLsnInt | Structure holding the listen interval configuration. |
References hif_send(), M2M_REQ_GROUP_WIFI, M2M_WIFI_REQ_LSN_INT, and NULL.
Referenced by os_m2m_wifi_set_lsn_int_imp().
Change the power profile mode
Not implemented in WINC3400 firmware.
Change the power profile mode.
[in] | u8PwrMode | Change the WINC power profile to different mode PWR_LOW1/PWR_LOW2/PWR_HIGH/PWR_AUTO (tenuM2mPwrMode) |
[in] | u8PwrMode | Change the WINC power profile to different mode based on the enumeration tenuM2mPwrMode. Not implemented in WINC3400 firmware. |
References hif_send(), M2M_REQ_GROUP_WIFI, M2M_SUCCESS, M2M_WIFI_REQ_SET_POWER_PROFILE, NULL, and tstrM2mPwrMode::u8PwrMode.
Set the power saving mode for the WINC3400.
Synchronous API to set the power-save mode of the WINC.
[in] | PsTyp | Desired power saving mode. Supported types are defined in tenuPowerSaveModes. |
[in] | BcastEn | Broadcast reception enable flag. If it is 1, the WINC3400 must be awake each DTIM Beacon for receiving Broadcast traffic. If it is 0, the WINC3400 will not wakeup at the DTIM Beacon, but its wakeup depends only on the the configured Listen Interval. |
This is one of the two synchronous power-save setting functions that allow the host MCU application to tweak the system power consumption. Such tweaking can be done through one of two ways: - 1) Changing the power save mode, to one of the allowed power save modes (see @ref tenuPowerSaveModes). This is done by setting the first parameter. - 2) Configuring DTIM monitoring: Configuring beacon monitoring parameters by enabling or disabling the reception of broadcast/multicast data. This is done by setting the second parameter.
[in] | PsTyp | Desired power saving mode. Supported types are enumerated in tenuPowerSaveModes. |
[in] | BcastEn | Broadcast reception enable flag. If set to 1, the WINC will wake for each DTIM beacon to ensure broadcast traffic can be received. If set to 0, the WINC will not wakeup at the DTIM beacon, ignoring broadcast traffic, instead it will wake every N beacon periods, as per the negotiated Listen Interval. |
References hif_send(), hif_set_sleep_mode(), M2M_INFO, M2M_REQ_GROUP_WIFI, M2M_SUCCESS, M2M_WIFI_REQ_SLEEP, NULL, tstrM2mPsType::u8BcastEn, and tstrM2mPsType::u8PsType.
Referenced by os_m2m_wifi_set_sleep_mode_imp().