Here are listed all the functions that implement the Wifi Roaming APIs.
Functions | |
sint8 | m2m_wifi_disable_roaming (void) |
Disable WiFi STA roaming. More... | |
sint8 | m2m_wifi_enable_roaming (uint8 bEnableDhcp) |
Enable WiFi STA roaming. More... | |
Disable WiFi STA roaming.
References hif_send(), M2M_REQ_GROUP_WIFI, M2M_WIFI_REQ_ROAMING, NULL, and tstrM2mWiFiRoaming::u8EnableRoaming.
Enable WiFi STA roaming.
m2m_wifi_enable_roaming enables the firmware to trigger the roaming algorithm/steps on link loss with the current AP. If roaming is successful, the @ref M2M_WIFI_RESP_CON_STATE_CHANGED message with state as @ref M2M_WIFI_ROAMED is sent to the host. Additionally a @ref M2M_WIFI_REQ_DHCP_CONF message with new DHCP lease details is sent to host (only if bEnableDhcp=1). If roaming is unsuccessful, a @ref M2M_WIFI_RESP_CON_STATE_CHANGED message with state as @ref M2M_WIFI_DISCONNECTED is sent to host.
[in] | bEnableDhcp | 0 : Disables DHCP client execution after roaming to new AP 1 : Enables DHCP client execution after roaming to new AP |
References hif_send(), M2M_ERR_INVALID_ARG, M2M_REQ_GROUP_WIFI, M2M_WIFI_REQ_ROAMING, NULL, tstrM2mWiFiRoaming::u8EnableDhcp, and tstrM2mWiFiRoaming::u8EnableRoaming.