Microchip® Advanced Software Framework

•All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Platform API

Functions

void platform_cmd_cmpl_signal (void)
 fires the command-complete signal More...
 
at_ble_status_t platform_cmd_cmpl_wait (void)
 blocks until the command-complete signal is fired More...
 
void platform_event_signal (void)
 fires the event signal More...
 
at_ble_status_t platform_event_wait (uint32_t timeout)
 blocks until the event signal is fired More...
 
at_ble_status_t platform_init (plf_params_t *platform_params)
 implements platform-specific initialization More...
 
void platform_interface_callback (uint8_t *data, uint32_t len)
 the callback to upper layers to process received packets More...
 
at_ble_status_t platform_interface_send (uint8_t *data, uint32_t len)
 sends a message over the platform-specific bus More...
 
void platform_receive (uint8_t *data, uint32_t len)
 
void platform_set_timeout (uint32_t timeout)
 set timeout value used for wait functions. More...
 

void platform_cmd_cmpl_signal ( void  )

fires the command-complete signal

Note
more details at the platform porting guide

References cmd_cmpl_flag.

Referenced by special_events_handler().

at_ble_status_t platform_cmd_cmpl_wait ( void  )

blocks until the command-complete signal is fired

Note
more details at the platform porting guide
Returns
non-zero if Timeout
zero if Operation completed successfully

References AT_BLE_FAILURE, AT_BLE_SUCCESS, cmd_cmpl_flag, gu32Jiffies1ms, gu32Timeout, and plf_params_t::plf_wait_cb.

Referenced by interface_send_wait().

void platform_event_signal ( void  )

fires the event signal

Note
more details at the platform porting guide

References event_flag.

Referenced by event_post().

at_ble_status_t platform_event_wait ( uint32_t  timeout)

blocks until the event signal is fired

Note
more details at the platform porting guide
Parameters
[in]timeouttimeout in ms passed by user

References AT_BLE_SUCCESS, AT_BLE_TIMEOUT, event_flag, gu32Jiffies1ms, and plf_params_t::plf_wait_cb.

Referenced by event_get().

at_ble_status_t platform_init ( plf_params_t platform_params)

implements platform-specific initialization

Parameters
[in]platform_paramsplatform specific params, this pointer is passed from the at_ble_init function and interpreted by the platform
Returns
AT_BLE_SUCCESS operation completed successfully
AT_BLE_FAILURE Generic error.

References AT_BLE_FW_INCOMPAT, AT_BLE_SUCCESS, plf_params_t::ble_write_cb, plf_params_t::fw_ver, plf_params_t::fw_version::major, MINIMUM_FW_MAJ, MINIMUM_FW_MIN, MINIMUM_FW_PATCH, plf_params_t::fw_version::minor, plf_params_t::mv, plf_params_t::fw_version::patch, plf_params_t::plf_wait_cb, and VERSION_FIELD_VALID.

Referenced by at_ble_init().

void platform_interface_callback ( uint8_t *  data,
uint32_t  len 
)

the callback to upper layers to process received packets

This function is implemented by the upper layers (the event loop) and it is up to the platform implementation to call it whenever data are received from the interface

Parameters
[in]datadata received from the interface
[in]lenlength of data

References event_post(), INTERFACE_API_PKT_ID, INTERFACE_HDR_LENGTH, INTERFACE_RCV_BUFF_LEN, INTERFACE_UNPACK_DONE, INTERFACE_UNPACK_INIT, INTERFACE_UNPACK_SKIP, INTERFACE_UNPACK_UINT16, NMI_BLE_COLLECTING_HDR, NMI_BLE_COLLECTING_PAYLOAD, NMI_BLE_WAITING, NULL, and special_events_handler().

Referenced by platform_receive().

at_ble_status_t platform_interface_send ( uint8_t *  data,
uint32_t  len 
)

sends a message over the platform-specific bus

Sends a message over the platform-specific bus that might be UART, SPI or other if the BTLC1000 external wakeup signal is used, it is up to this function implementation to assert/deassert it appropriately

Parameters
[in]datadata to send over the interface
[in]lenlength of data
Returns
Zero if operation completed successfully
Non zero for Generic error.

References AT_BLE_FAILURE, AT_BLE_SUCCESS, and plf_params_t::ble_write_cb.

Referenced by interface_send().

void platform_receive ( uint8_t *  data,
uint32_t  len 
)
void platform_set_timeout ( uint32_t  timeout)

set timeout value used for wait functions.

Note
more details at the platform porting guide
Parameters
[in]timeouttimeout in ms passed by user

References gu32Timeout.