Microchip® Advanced Software Framework

tstrI2cMasterInitParam Struct Reference

I2C master configuration parameters.

See Also
tenuI2cMasterSclMuxOpt tenuI2cMasterSdaMuxOpt

#include <m2m_periph.h>

Data Fields

uint8 enuSclMuxOpt
 
uint8 enuSdaMuxOpt
 
uint8 u8ClkSpeedKHz
 

uint8 tstrI2cMasterInitParam::enuSclMuxOpt

SCL multiplexing option. Allowed value are defined in tenuI2cMasterSclMuxOpt

uint8 tstrI2cMasterInitParam::enuSdaMuxOpt

SDA multiplexing option. Allowed value are defined in tenuI2cMasterSdaMuxOpt

uint8 tstrI2cMasterInitParam::u8ClkSpeedKHz

I2C master clock speed in KHz.