Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
System Time

        Here are listed all the functions that implement the System Time APIs.

Functions

sint8 m2m_wifi_configure_sntp (uint8 *pu8NTPServerName, uint8 u8NTPServerNameLength, tenuSNTPUseDHCP useDHCP)
 Configures what NTP server the SNTP client should use. More...
 
sint8 m2m_wifi_enable_sntp (uint8 bEnable)
 Asynchronous API to enable or disable the native Simple Network Time Protocol(SNTP) client running on the WINC. More...
 
sint8 m2m_wifi_get_system_time (void)
 Asynchronous API to obtain the system time in use by the WINC. More...
 
sint8 m2m_wifi_set_system_time (uint32 u32UTCSeconds)
 Asynchronous function for setting the system time within the WINC. More...
 

NMI_API sint8 m2m_wifi_configure_sntp ( uint8 pu8NTPServerName,
uint8  u8NTPServerNameLength,
tenuSNTPUseDHCP  useDHCP 
)

Configures what NTP server the SNTP client should use.

Parameters
[in]pu8NTPServerNameBuffer holding the NTP server name. If the first character is an asterisk (*) then it will be treated as a server pool, where the asterisk will be replaced with an incrementing value from 0 to 3 each time a server fails (example: *.pool.ntp.org).
[in]u8NTPServerNameLengthLength of the NTP server name. Should not exceed the maximum NTP server name length of M2M_NTP_MAX_SERVER_NAME_LENGTH
[in]useDHCPShould the NTP server provided by the DHCP server be used.
Returns
The function SHALL return M2M_SUCCESS for success and a negative value otherwise.
Configures what NTP server the SNTP client should use. Only 1 server name can be provided, if the configured server name begins with an asterisk then it will be treated as a server pool.
The SNTP client can also use the NTP server provided by the DHCP server through option 42.
By default the NTP server provided by DHCP will be tried first, then the built-in default NTP server (time.nist.gov) will be used.
Parameters
[in]pu8NTPServerNameBuffer holding the NTP server name. If the first character is an asterisk (*) then it will be treated as a server pool, where the asterisk will be replaced with an incrementing value from 0 to 3 each time a server fails (example: *.pool.ntp.org).
[in]u8NTPServerNameLengthLength of the NTP server name. Should not exceed the maximum NTP server name length of M2M_NTP_MAX_SERVER_NAME_LENGTH.
[in]useDHCPExplicity tell the WINC if it should use the NTP server provided by the DHCP server or not.
Warning
SNTP should be configured before the connection takes place. If SNTP is configured after the device connects to a network, the new configuration can take a minimum of 24h to be applied. However, it can take even longer since it is triggered by DHCP renewal. Currently there is also a known issue in which if the WINC obtains the NTP server from DHCP and then connects to a different network, it will still use the NTP from the previous network. Configuring a server name will overwrite the built-in default server until next reboot.
Returns
The function returns M2M_SUCCESS for success and a negative value otherwise.

References tstrM2MSNTPConfig::acNTPServer, tstrM2MSNTPConfig::enuUseDHCP, hif_send(), M2M_ERR_FAIL, m2m_memcpy(), M2M_NTP_MAX_SERVER_NAME_LENGTH, M2M_REQ_GROUP_WIFI, M2M_WIFI_REQ_CONFIG_SNTP, and NULL.

NMI_API sint8 m2m_wifi_enable_sntp ( uint8  bEnable)

Asynchronous API to enable or disable the native Simple Network Time Protocol(SNTP) client running on the WINC.

The SNTP client is enabled by default during chip initialization. This function can be used to
disable or subsequently re-enable the service.

The service is capable of synchronizing the WINC system clock to the UTC time from a well-known
(and trusted) time server, for example "time.nist.gov". By default the SNTP client will update the
system time once every 24 hours. The ability to track the time accurately is important for various
applications such as checking expiry of X509 certificates during TLS (Transport Layer Security)
session establishment.

It is highly recommended to leave SNTP enabled if there is no alternative source of timing
information. For systems including an RTC device, SNTP may not be needed and the WINC's time
may be set using the @ref m2m_wifi_set_system_time function.
Parameters
[in]bEnableEnables or disables the SNTP service '0' :disable SNTP '1' :enable SNTP
Returns
The function returns M2M_SUCCESS if the command has been successfully queued to the WINC and a negative value otherwise.
See Also
m2m_wifi_set_system_time

References hif_send(), M2M_REQ_GROUP_WIFI, M2M_WIFI_REQ_DISABLE_SNTP_CLIENT, M2M_WIFI_REQ_ENABLE_SNTP_CLIENT, and NULL.

NMI_API sint8 m2m_wifi_get_system_time ( void  )

Asynchronous API to obtain the system time in use by the WINC.

See Also
m2m_wifi_enable_sntp tstrSystemTime
Note
get the system time from the sntp client using the API m2m_wifi_get_system_time.
Returns
The function returns M2M_SUCCESS for successful operations and a negative value otherwise.
This function will request the WINC to report its current system time to the application. The
information will arrive at the application via the @ref tpfAppWifiCb and event @ref M2M_WIFI_RESP_GET_SYS_TIME.
Response time retrieved is parsed into the members defined in the structure @ref tstrSystemTime.
Note
Returns
The function returns M2M_SUCCESS if the command has been successfully queued to the WINC and a negative value otherwise.
See Also
m2m_wifi_enable_sntp tstrSystemTime

References hif_send(), M2M_REQ_GROUP_WIFI, M2M_WIFI_REQ_GET_SYS_TIME, and NULL.

NMI_API sint8 m2m_wifi_set_system_time ( uint32  u32UTCSeconds)

Asynchronous function for setting the system time within the WINC.

Function for setting the system time in time/date format (@ref uint32).
The @ref tstrSystemTime structure can be used as a reference to the time values that
should be set and pass its value as @ref uint32.
Parameters
[in]u32UTCSecondsSeconds elapsed since January 1, 1900 (NTP Timestamp).
Returns
The function returns M2M_SUCCESS if the command has been successfully queued to the WINC and a negative value otherwise.
See Also
m2m_wifi_enable_sntp tstrSystemTime
Note
If there is an RTC on the host MCU, the SNTP may be disabled and the host may set the system time within the firmware using the API m2m_wifi_set_system_time.

References hif_send(), M2M_REQ_GROUP_WIFI, M2M_WIFI_REQ_SET_SYS_TIME, and NULL.