Microchip® Advanced Software Framework

flash_efc.h File Reference

Embedded Flash service for SAM.

Copyright (c) 2011-2019 Microchip Technology Inc. and its subsidiaries.

#include "compiler.h"
#include "efc.h"

Macros

Flash access mode
#define FLASH_ACCESS_MODE_128   EFC_ACCESS_MODE_128
 
#define FLASH_ACCESS_MODE_64   EFC_ACCESS_MODE_64
 

Functions

uint32_t flash_clear_gpnvm (uint32_t ul_gpnvm)
 Clear the given GPNVM bit. More...
 
uint32_t flash_enable_security_bit (void)
 Set security bit. More...
 
uint32_t flash_erase_all (uint32_t ul_address)
 Erase the entire flash. More...
 
uint32_t flash_erase_page (uint32_t ul_address, uint8_t uc_page_num)
 
uint32_t flash_erase_plane (uint32_t ul_address)
 
uint32_t flash_erase_sector (uint32_t ul_address)
 
uint32_t flash_erase_user_signature (void)
 
uint32_t flash_get_descriptor (uint32_t ul_address, uint32_t *pul_flash_descriptor, uint32_t ul_size)
 Get flash descriptor. More...
 
uint32_t flash_get_page_count (const uint32_t *pul_flash_descriptor)
 Get flash total page count for the specified bank. More...
 
uint32_t flash_get_page_count_per_region (const uint32_t *pul_flash_descriptor)
 Get flash page count per region (plane) for the specified bank. More...
 
uint32_t flash_get_region_count (const uint32_t *pul_flash_descriptor)
 Get flash region (plane) count for the specified bank. More...
 
uint32_t flash_get_wait_state (uint32_t ul_address)
 Get flash wait state. More...
 
uint32_t flash_init (uint32_t ul_mode, uint32_t ul_fws)
 Initialize the flash service. More...
 
uint32_t flash_is_gpnvm_set (uint32_t ul_gpnvm)
 Check if the given GPNVM bit is set or not. More...
 
uint32_t flash_is_locked (uint32_t ul_start, uint32_t ul_end)
 Get the number of locked regions inside the given address range. More...
 
uint32_t flash_is_security_bit_enabled (void)
 Check if the security bit is set or not. More...
 
uint32_t flash_lock (uint32_t ul_start, uint32_t ul_end, uint32_t *pul_actual_start, uint32_t *pul_actual_end)
 Lock all the regions in the given address range. More...
 
uint32_t flash_read_unique_id (uint32_t *pul_data, uint32_t ul_size)
 Read the flash unique ID. More...
 
uint32_t flash_read_user_signature (uint32_t *p_data, uint32_t ul_size)
 
uint32_t flash_set_gpnvm (uint32_t ul_gpnvm)
 Set the given GPNVM bit. More...
 
uint32_t flash_set_wait_state (uint32_t ul_address, uint32_t ul_fws)
 Set flash wait state. More...
 
uint32_t flash_set_wait_state_adaptively (uint32_t ul_address)
 Set flash wait state. More...
 
uint32_t flash_unlock (uint32_t ul_start, uint32_t ul_end, uint32_t *pul_actual_start, uint32_t *pul_actual_end)
 Unlock all the regions in the given address range. More...
 
uint32_t flash_write (uint32_t ul_address, const void *p_buffer, uint32_t ul_size, uint32_t ul_erase_flag)
 Write a data buffer on flash. More...
 
uint32_t flash_write_user_signature (const void *p_buffer, uint32_t ul_size)
 

Flash driver return codes

enum  flash_rc {
  FLASH_RC_OK = 0,
  FLASH_RC_YES = 1,
  FLASH_RC_NO = 0,
  FLASH_RC_ERROR = 0x10,
  FLASH_RC_INVALID,
  FLASH_RC_NOT_SUPPORT = 0xFFFFFFFF
}
 
typedef enum flash_rc flash_rc_t
 

Flash erase page num in FARG[1:0]

Note
The erase page commands should be cautiouly used as EPA4/EPA32 will not take effect according to errata and EPA8/EPA16 must module 8/16 page addresses.
enum  flash_farg_page_num {
  IFLASH_ERASE_PAGES_4 =0,
  IFLASH_ERASE_PAGES_8,
  IFLASH_ERASE_PAGES_16,
  IFLASH_ERASE_PAGES_32,
  IFLASH_ERASE_PAGES_INVALID
}
 
typedef enum flash_farg_page_num flash_farg_page_num_t
 

#define FLASH_ACCESS_MODE_128   EFC_ACCESS_MODE_128
#define FLASH_ACCESS_MODE_64   EFC_ACCESS_MODE_64

typedef enum flash_rc flash_rc_t

Enumerator
IFLASH_ERASE_PAGES_4 
IFLASH_ERASE_PAGES_8 
IFLASH_ERASE_PAGES_16 
IFLASH_ERASE_PAGES_32 
IFLASH_ERASE_PAGES_INVALID 
enum flash_rc
Enumerator
FLASH_RC_OK 

Operation OK.

FLASH_RC_YES 

Yes.

FLASH_RC_NO 

No.

FLASH_RC_ERROR 

General error.

FLASH_RC_INVALID 

Invalid argument input.

FLASH_RC_NOT_SUPPORT 

Operation is not supported.

uint32_t flash_erase_page ( uint32_t  ul_address,
uint8_t  uc_page_num 
)

Referenced by nvm_page_erase().

uint32_t flash_erase_plane ( uint32_t  ul_address)
uint32_t flash_erase_sector ( uint32_t  ul_address)
uint32_t flash_erase_user_signature ( void  )

Referenced by nvm_page_erase().

uint32_t flash_read_user_signature ( uint32_t *  p_data,
uint32_t  ul_size 
)

Referenced by nvm_read(), and nvm_read_char().

uint32_t flash_write_user_signature ( const void *  p_buffer,
uint32_t  ul_size 
)

Referenced by nvm_write(), and nvm_write_char().