This is the unit test application for the Common Clock service. It consists of test cases for the following:
All AVR and SAM4L devices can be used. This example has been tested with the following setup:
See the documentation for the individual unit test functions here for detailed descriptions of the tests.
This example depends directly on the following modules:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.
Support and FAQ: https://www.microchip.com/support/