This is the unit test application for the FIFO service. It consists of test cases for the following:
All Atmel devices can be used.
See the documentation for the individual unit test functions here for detailed descriptions of the tests.
This example depends directly on the following modules:
This software was written for the GNU GCC and IAR for AVR or ARM. Other compilers may or may not work.
For further information, visit Microchip.