Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
SPI Master Mode Example for atmega128rfa1_stk600-rc128x_rfx Documentation

Introduction

This example demonstrates how to use the SPI Master Mode Basic Services.

Main Files

services/basic/spi API

The spi API can be found here.

Device Info

All AVR devices can be used. This example has been tested with the following setup:

  • Evaluation kits with a dataflash connecting through a SPI interface. To make this example work on STK600 define AT45DB041 in config file.

Description of the example

Compilation Info

This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.

Contact Information

For further information, visit Microchip.