License | Subject to your compliance with these terms, you may use Microchip software and any derivatives exclusively with Microchip products |
Quick start guide for the SAM PMC module | This is the quick start guide for the PMC module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick Start Guide for the System Clock Management service (SAM3A) | This is the quick start guide for the System Clock Management service, with step-by-step instructions on how to configure and use the service for specific use cases |
Quick start guide for Serial Interface service | This is the quick start guide for the Serial Interface module, with step-by-step instructions on how to configure and use the serial in a selection of use cases |
 Advanced use case - Send a packet of serial data | In this use case, the USART module is configured for: |
Quick start guide for the SAM USART module | This is the quick start guide for the USART module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
 USART receive character and echo back | In this use case, the USART module is configured for: |
 USART receive character and echo back via interrupts | In this use case, the USART module is configured for: |
Quick start guide for the common IOPORT service | This is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases |
 Advanced use case doing port access | In this case we will read out the pins from one whole port and write the read value to another port |
Extra Information for Peripheral DMA Controller | |
Examples for Peripheral DMA Controller | This is a list of the available Quick Start guides (QSGs) and example applications for SAM3A/3N/3S/3U/3X/4E/4N/4S/G Peripheral DMA Controller (PDC) Driver |
 Quick Start Guide for PDC - Basic | This is the quickstart guide for SAM3A/3N/3S/3U/3X/4E/4N/4S/G Peripheral DMA Controller (PDC) Driver with step-by-step instructions on how to configure and use the driver |
 Peripheral DMA Controller Example | |
Document Revision History | |
Quick start guide for USB device Communication Class Device module (UDI CDC) | This is the quick start guide for the USB device interface CDC module (UDI CDC) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 CDC in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
 Change USB speed | In this use case, the USB device is used with different USB speeds |
 Use USB strings | In this use case, the usual USB strings is added in the USB device |
 Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
 Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
 USB dynamic serial number | In this use case, the USB serial strings is dynamic |
conf_clock.h examples with USB support | Content of XMEGA conf_clock.h: |
Quick Start Guide for the SAM PIO driver | This is the quick start guide for the PIO Driver, with step-by-step instructions on how to configure and use the driver for specific use cases |
Advanced use case - Interrupt driven edge detection | |
Quick start guide for | FreeRTOS TWI peripheral control functions |
 Initializing the FreeRTOS TWI driver | For standard operation |
 Transmitting using the FreeRTOS TWI driver in | Standard mode |
 Receiving using the FreeRTOS TWI driver in | Standard mode |
 Initializing the FreeRTOS TWI driver | For asynchronous operation |
 Transmitting using the FreeRTOS TWI driver in | Fully asynchronous mode |
 Receiving using the FreeRTOS TWI driver in fully | Asynchronous mode |
Quickstart guide for Common service TWI | This is the quickstart guide for the Common service TWI, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick start guide for | FreeRTOS USART peripheral control functions |
 Initializing the FreeRTOS USART | Driver for standard operation |
 Transmitting using the FreeRTOS USART driver in | Standard mode |
 Initializing the FreeRTOS USART | Driver for asynchronous operation |
 Transmitting using the FreeRTOS USART driver in | Fully asynchronous mode |
 Receiving using the FreeRTOS USART driver | This example demonstrates using the FreeRTOS USART API to receive data |
Quick start guide for | FreeRTOS UART peripheral control functions |
 Initializing the FreeRTOS UART | Driver for standard operation |
 Transmitting using the FreeRTOS UART driver in | Standard mode |
 Initializing the FreeRTOS UART | Driver for asynchronous operation |
 Transmitting using the FreeRTOS UART driver in | Fully asynchronous mode |
 Receiving using the FreeRTOS UART driver | This example demonstrates using the FreeRTOS UART API to receive data |
"Arduino Due/X - Operating frequencies" | This page lists several definition related to the board operating frequency |
"Arduino Due/X - Board informations" | This page lists several definition related to the board description |
"Arduino Due/X - PIO definitions" | This pages lists all the pio definitions |
Todo List | |