See Quick start guide for the common IOPORT service.
This is common IOPORT service for GPIO pin configuration and control in a standardized manner across the MEGA, MEGA_RF, XMEGA, UC3 and ARM devices.
Port pin control code is optimized for each platform, and should produce both compact and fast execution times when used with constant values.
This driver depends on the following modules:
For details on these please see the SAM Manual.
Macros | |
#define | IOPORT_CREATE_PIN(port, pin) ((IOPORT_ ## port) * 32 + (pin)) |
Create IOPORT pin number. More... | |
Enumerations | |
enum | ioport_direction { IOPORT_DIR_INPUT, IOPORT_DIR_OUTPUT } |
IOPORT pin directions. More... | |
enum | ioport_sense { IOPORT_SENSE_BOTHEDGES, IOPORT_SENSE_RISING, IOPORT_SENSE_FALLING } |
enum | ioport_value { IOPORT_PIN_LEVEL_LOW, IOPORT_PIN_LEVEL_HIGH } |
IOPORT levels. More... | |
Functions | |
static void | ioport_disable_pin (ioport_pin_t pin) |
Disable IOPORT pin, based on a pin created with IOPORT_CREATE_PIN(). More... | |
static void | ioport_disable_port (ioport_port_t port, ioport_port_mask_t mask) |
Disable multiple pins in a single IOPORT port. More... | |
static void | ioport_enable_pin (ioport_pin_t pin) |
Enable an IOPORT pin, based on a pin created with IOPORT_CREATE_PIN(). More... | |
static void | ioport_enable_port (ioport_port_t port, ioport_port_mask_t mask) |
Enable multiple pins in a single IOPORT port. More... | |
static bool | ioport_get_pin_level (ioport_pin_t pin) |
Get current value of an IOPORT pin, which has been configured as an input. More... | |
static ioport_port_mask_t | ioport_get_port_level (ioport_pin_t port, ioport_port_mask_t mask) |
Get current value of several IOPORT pins in a single port, which have been configured as an inputs. More... | |
static void | ioport_init (void) |
Initializes the IOPORT service, ready for use. More... | |
static ioport_port_mask_t | ioport_pin_to_mask (ioport_pin_t pin) |
Convert a pin ID into a bitmask mask for the given pin on its port. More... | |
static ioport_port_t | ioport_pin_to_port_id (ioport_pin_t pin) |
Convert a pin ID into a its port ID. More... | |
static void | ioport_reset_pin_mode (ioport_pin_t pin) |
Reset pin mode configuration for a single IOPORT pin. More... | |
static void | ioport_reset_port_mode (ioport_port_t port, ioport_port_mask_t mask) |
Reset multiple pin modes in a specified IOPORT port to defaults. More... | |
static void | ioport_set_pin_dir (ioport_pin_t pin, enum ioport_direction dir) |
Set direction for a single IOPORT pin. More... | |
static void | ioport_set_pin_level (ioport_pin_t pin, bool level) |
Set an IOPORT pin to a specified logical value. More... | |
static void | ioport_set_pin_mode (ioport_pin_t pin, ioport_mode_t mode) |
Set pin mode for one single IOPORT pin. More... | |
static void | ioport_set_pin_sense_mode (ioport_pin_t pin, enum ioport_sense pin_sense) |
Set the pin sense mode of a single IOPORT pin. More... | |
static void | ioport_set_port_dir (ioport_port_t port, ioport_port_mask_t mask, enum ioport_direction dir) |
Set I/O direction for a group of pins in a single IOPORT. More... | |
static void | ioport_set_port_level (ioport_port_t port, ioport_port_mask_t mask, enum ioport_value level) |
Set a group of IOPORT pins in a single port to a specified logical value. More... | |
static void | ioport_set_port_mode (ioport_port_t port, ioport_port_mask_t mask, ioport_mode_t mode) |
Set multiple pin modes in a single IOPORT port, such as pull-up, pull-down, etc. More... | |
static void | ioport_set_port_sense_mode (ioport_port_t port, ioport_port_mask_t mask, enum ioport_sense pin_sense) |
Set the pin sense mode of a multiple IOPORT pins on a single port. More... | |
static void | ioport_toggle_pin_level (ioport_pin_t pin) |
Toggle the value of an IOPORT pin, which has previously configured as an output. More... | |
static void | ioport_toggle_port_level (ioport_port_t port, ioport_port_mask_t mask) |
Toggle the values of several IOPORT pins located in a single port. More... | |
IOPORT Mode bit definitions | |
#define | IOPORT_MODE_MUX_MASK (0x7 << 0) |
#define | IOPORT_MODE_MUX_BIT0 ( 1 << 0) |
#define | IOPORT_MODE_MUX_BIT1 ( 1 << 1) |
#define | IOPORT_MODE_MUX_A ( 0 << 0) |
#define | IOPORT_MODE_MUX_B ( 1 << 0) |
#define | IOPORT_MODE_MUX_C ( 2 << 0) |
#define | IOPORT_MODE_MUX_D ( 3 << 0) |
#define | IOPORT_MODE_PULLUP ( 1 << 3) |
#define | IOPORT_MODE_PULLDOWN ( 1 << 4) |
#define | IOPORT_MODE_OPEN_DRAIN ( 1 << 5) |
#define | IOPORT_MODE_GLITCH_FILTER ( 1 << 6) |
#define | IOPORT_MODE_DEBOUNCE ( 1 << 7) |
#define IOPORT_CREATE_PIN | ( | port, | |
pin | |||
) | ((IOPORT_ ## port) * 32 + (pin)) |
Create IOPORT pin number.
Create a IOPORT pin number for use with the IOPORT functions.
port | IOPORT port (e.g. PORTA, PA or PIOA depending on chosen architecture) |
pin | IOPORT zero-based index of the I/O pin |
#define IOPORT_MODE_DEBOUNCE ( 1 << 7) |
Input debounce
Referenced by arch_ioport_set_port_mode().
#define IOPORT_MODE_GLITCH_FILTER ( 1 << 6) |
Glitch filter
Referenced by arch_ioport_set_port_mode().
#define IOPORT_MODE_MUX_A ( 0 << 0) |
MUX function A
#define IOPORT_MODE_MUX_B ( 1 << 0) |
MUX function B
#define IOPORT_MODE_MUX_BIT0 ( 1 << 0) |
MUX BIT0 mask
Referenced by arch_ioport_set_port_mode().
#define IOPORT_MODE_MUX_BIT1 ( 1 << 1) |
MUX BIT1 mask
Referenced by arch_ioport_set_port_mode().
#define IOPORT_MODE_MUX_C ( 2 << 0) |
MUX function C
#define IOPORT_MODE_MUX_D ( 3 << 0) |
MUX function D
#define IOPORT_MODE_MUX_MASK (0x7 << 0) |
MUX bits mask
#define IOPORT_MODE_OPEN_DRAIN ( 1 << 5) |
Open drain
Referenced by arch_ioport_set_port_mode().
#define IOPORT_MODE_PULLDOWN ( 1 << 4) |
Pull-down
Referenced by arch_ioport_set_port_mode().
#define IOPORT_MODE_PULLUP ( 1 << 3) |
Pull-up
Referenced by arch_ioport_set_port_mode().
enum ioport_direction |
enum ioport_sense |
enum ioport_value |
|
inlinestatic |
Disable IOPORT pin, based on a pin created with IOPORT_CREATE_PIN().
pin | IOPORT pin to disable |
References arch_ioport_disable_pin().
Referenced by at24cxx_reset().
|
inlinestatic |
Disable multiple pins in a single IOPORT port.
port | IOPORT port to disable |
mask | Pin mask of pins to disable |
References arch_ioport_disable_port().
|
inlinestatic |
Enable an IOPORT pin, based on a pin created with IOPORT_CREATE_PIN().
pin | IOPORT pin to enable |
References arch_ioport_enable_pin().
Referenced by at24cxx_reset().
|
inlinestatic |
Enable multiple pins in a single IOPORT port.
port | IOPORT port to enable |
mask | Mask of pins within the port to enable |
References arch_ioport_enable_port().
|
inlinestatic |
Get current value of an IOPORT pin, which has been configured as an input.
pin | IOPORT pin to read |
References arch_ioport_get_pin_level().
|
inlinestatic |
Get current value of several IOPORT pins in a single port, which have been configured as an inputs.
port | IOPORT port to read |
mask | Pin mask of pins to read |
References arch_ioport_get_port_level().
|
inlinestatic |
Initializes the IOPORT service, ready for use.
This function must be called before using any other functions in the IOPORT service.
References arch_ioport_init().
Referenced by board_init().
|
inlinestatic |
Convert a pin ID into a bitmask mask for the given pin on its port.
pin | IOPORT pin ID to convert |
Bitmask | with a bit set that corresponds to the given pin ID in its port |
References arch_ioport_pin_to_mask().
|
inlinestatic |
Convert a pin ID into a its port ID.
pin | IOPORT pin ID to convert |
Port | ID for the given pin ID |
References arch_ioport_pin_to_port_id().
|
inlinestatic |
Reset pin mode configuration for a single IOPORT pin.
pin | IOPORT pin to configure |
References arch_ioport_set_pin_mode().
|
inlinestatic |
Reset multiple pin modes in a specified IOPORT port to defaults.
port | IOPORT port to configure |
mask | Mask of pins whose mode configuration is to be reset |
References arch_ioport_set_port_mode().
|
inlinestatic |
Set direction for a single IOPORT pin.
pin | IOPORT pin to configure |
dir | Direction to set for the specified pin (ioport_direction) |
References arch_ioport_set_pin_dir().
Referenced by at24cxx_reset().
|
inlinestatic |
Set an IOPORT pin to a specified logical value.
pin | IOPORT pin to configure |
level | Logical value of the pin |
References arch_ioport_set_pin_level().
Referenced by at24cxx_reset().
|
inlinestatic |
Set pin mode for one single IOPORT pin.
pin | IOPORT pin to configure |
mode | Mode masks to configure for the specified pin (IOPORT Modes) |
References arch_ioport_set_pin_mode().
Referenced by at24cxx_reset().
|
inlinestatic |
Set the pin sense mode of a single IOPORT pin.
pin | IOPORT pin to configure |
pin_sense | Edge to sense for the pin (ioport_sense) |
References arch_ioport_set_pin_sense_mode().
|
inlinestatic |
Set I/O direction for a group of pins in a single IOPORT.
port | IOPORT port to configure |
mask | Pin mask of pins to configure |
dir | Direction to set for the specified pins (ioport_direction) |
References arch_ioport_set_port_dir().
|
inlinestatic |
Set a group of IOPORT pins in a single port to a specified logical value.
port | IOPORT port to write to |
mask | Pin mask of pins to modify |
level | Level of the pins to be modified |
References arch_ioport_set_port_level().
|
inlinestatic |
Set multiple pin modes in a single IOPORT port, such as pull-up, pull-down, etc.
configuration.
port | IOPORT port to configure |
mask | Pin mask of pins to configure |
mode | Mode masks to configure for the specified pins (IOPORT Modes) |
References arch_ioport_set_port_mode().
|
inlinestatic |
Set the pin sense mode of a multiple IOPORT pins on a single port.
port | IOPORT port to configure |
mask | Bitmask if pins whose edge sense is to be configured |
pin_sense | Edge to sense for the pins (ioport_sense) |
References arch_ioport_set_port_sense_mode().
|
inlinestatic |
Toggle the value of an IOPORT pin, which has previously configured as an output.
pin | IOPORT pin to toggle |
References arch_ioport_toggle_pin_level().
|
inlinestatic |
Toggle the values of several IOPORT pins located in a single port.
port | IOPORT port to modify |
mask | Pin mask of pins to toggle |
References arch_ioport_toggle_port_level().