Microchip® Advanced Software Framework

•All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
XMEGA SPI master service.

This is the API for SPI master service on XMEGA.

Quick Start Guide

See Quick Start Guide for the SPI Master Driver

Data Structures

struct  spi_device
 Polled SPI device definition. More...
 

Macros

#define SPI_CPHA   (1 << 0)
 Clock phase. More...
 
#define SPI_CPOL   (1 << 1)
 Clock polarity. More...
 
#define SPI_MODE_0   0
 SPI mode 0. More...
 
#define SPI_MODE_1   (SPI_CPHA)
 SPI mode 1. More...
 
#define SPI_MODE_2   (SPI_CPOL)
 SPI mode 2. More...
 
#define SPI_MODE_3   (SPI_CPOL | SPI_CPHA)
 SPI mode 3. More...
 

Typedefs

typedef uint32_t board_spi_select_id_t
 
typedef uint8_t spi_flags_t
 

Functions

void spi_deselect_device (SPI_t *spi, struct spi_device *device)
 Deselect given device on the SPI bus. More...
 
void spi_disable (SPI_t *spi)
 Disables the SPI. More...
 
void spi_enable (SPI_t *spi)
 Enables the SPI. More...
 
bool spi_is_enabled (SPI_t *spi)
 Tests if the SPI is enabled. More...
 
static bool spi_is_rx_full (SPI_t *spi)
 Tests if the SPI contains a received character. More...
 
static bool spi_is_rx_ready (SPI_t *spi)
 Checks if all reception is ready. More...
 
static bool spi_is_tx_empty (SPI_t *spi)
 Checks if all transmissions are complete. More...
 
static bool spi_is_tx_ready (SPI_t *spi)
 Checks if all transmissions is ready. More...
 
void spi_master_init (SPI_t *spi)
 Initializes the SPI in master mode. More...
 
void spi_master_setup_device (SPI_t *spi, struct spi_device *device, spi_flags_t flags, unsigned long baud_rate, board_spi_select_id_t sel_id)
 Setup a SPI device. More...
 
status_code_t spi_read_packet (SPI_t *spi, uint8_t *data, size_t len)
 Receive a sequence of bytes from a SPI device. More...
 
static void spi_read_single (SPI_t *spi, uint8_t *data)
 Receive one byte from a SPI device. More...
 
void spi_select_device (SPI_t *spi, struct spi_device *device)
 Select given device on the SPI bus. More...
 
status_code_t spi_write_packet (SPI_t *spi, const uint8_t *data, size_t len)
 Send a sequence of bytes to a SPI device. More...
 
static __always_inline void spi_write_single (SPI_t *spi, uint8_t data)
 Write one byte to a SPI device. More...
 

Spi Master Management Configuration

#define CONFIG_SPI_MASTER_DUMMY   0xFF
 Default Config Spi Master Dummy Field. More...
 

#define CONFIG_SPI_MASTER_DUMMY   0xFF

Default Config Spi Master Dummy Field.

Referenced by spi_read_packet().

#define SPI_CPHA   (1 << 0)

Clock phase.

#define SPI_CPOL   (1 << 1)

Clock polarity.

#define SPI_MODE_0   0

SPI mode 0.

Referenced by ssd1306_interface_init().

#define SPI_MODE_1   (SPI_CPHA)

SPI mode 1.

#define SPI_MODE_2   (SPI_CPOL)

SPI mode 2.

#define SPI_MODE_3   (SPI_CPOL | SPI_CPHA)

SPI mode 3.

typedef uint32_t board_spi_select_id_t
typedef uint8_t spi_flags_t

void spi_deselect_device ( SPI_t *  spi,
struct spi_device device 
)

Deselect given device on the SPI bus.

Calls board chip deselect.

Parameters
spiBase address of the SPI instance.
deviceSPI device
Precondition
SPI device must be selected with spi_select_device() first

References spi_device::id, and ioport_set_pin_high().

Referenced by ssd1306_write_command(), and ssd1306_write_data().

void spi_disable ( SPI_t *  spi)

Disables the SPI.

Ensures that nothing is transferred while setting up buffers.

Parameters
spiBase address of the SPI instance.
Warning
This may cause data loss if used on a slave SPI.
void spi_enable ( SPI_t *  spi)

Enables the SPI.

Parameters
spiBase address of the SPI instance.

Referenced by ssd1306_interface_init().

bool spi_is_enabled ( SPI_t *  spi)

Tests if the SPI is enabled.

Parameters
spiBase address of the SPI instance.
Returns
1 if the SPI is enabled, otherwise 0.
static bool spi_is_rx_full ( SPI_t *  spi)
inlinestatic

Tests if the SPI contains a received character.

Parameters
spiBase address of the SPI instance.
Returns
1 if the SPI Receive Holding Register is full, otherwise 0.

References spi_is_tx_ok().

Referenced by spi_read_packet(), and spi_write_packet().

static bool spi_is_rx_ready ( SPI_t *  spi)
inlinestatic

Checks if all reception is ready.

Parameters
spiBase address of the SPI instance.
Returns
1 if the SPI Receiver is ready, otherwise 0.

References spi_is_tx_ok().

static bool spi_is_tx_empty ( SPI_t *  spi)
inlinestatic

Checks if all transmissions are complete.

Parameters
spiBase address of the SPI instance.
Returns
Status.
Return values
1All transmissions complete.
0Transmissions not complete.

References spi_is_tx_ok().

static bool spi_is_tx_ready ( SPI_t *  spi)
inlinestatic

Checks if all transmissions is ready.

Parameters
spiBase address of the SPI instance.
Returns
Status.
Return values
1All transmissions complete.
0Transmissions not complete.

References spi_is_tx_ok().

void spi_master_init ( SPI_t *  spi)

Initializes the SPI in master mode.

Parameters
spiBase address of the SPI instance.

References spi_enable_master_mode(), sysclk_enable_module(), SYSCLK_PORT_A, SYSCLK_PORT_B, SYSCLK_PORT_C, SYSCLK_PORT_D, SYSCLK_PORT_E, and SYSCLK_PORT_F.

Referenced by ssd1306_interface_init().

void spi_master_setup_device ( SPI_t *  spi,
struct spi_device device,
spi_flags_t  flags,
unsigned long  baud_rate,
board_spi_select_id_t  sel_id 
)

Setup a SPI device.

The returned device descriptor structure must be passed to the driver whenever that device should be used as current slave device.

Parameters
spiBase address of the SPI instance.
devicePointer to SPI device struct that should be initialized.
flagsSPI configuration flags. Common flags for all implementations are the SPI modes SPI_MODE_0 ... SPI_MODE_3.
baud_rateBaud rate for communication with slave device in Hz.
sel_idBoard specific select id
status_code_t spi_read_packet ( SPI_t *  spi,
uint8_t *  data,
size_t  len 
)

Receive a sequence of bytes from a SPI device.

All bytes sent out on SPI bus are sent as value 0.

Parameters
spiBase address of the SPI instance.
datadata buffer to read
lenLength of data
Precondition
SPI device must be selected with spi_select_device() first

References CONFIG_SPI_MASTER_DUMMY, spi_is_rx_full(), spi_read_single(), spi_write_single(), and STATUS_OK.

static void spi_read_single ( SPI_t *  spi,
uint8_t *  data 
)
inlinestatic

Receive one byte from a SPI device.

Parameters
spiBase address of the SPI instance.
dataPointer to the data byte where to store the received data.

References spi_get().

Referenced by spi_read_packet().

void spi_select_device ( SPI_t *  spi,
struct spi_device device 
)

Select given device on the SPI bus.

Set device specific setting and calls board chip select.

Parameters
spiBase address of the SPI instance.
deviceSPI device

References spi_device::id, and ioport_set_pin_low().

Referenced by ssd1306_write_command(), and ssd1306_write_data().

status_code_t spi_write_packet ( SPI_t *  spi,
const uint8_t *  data,
size_t  len 
)

Send a sequence of bytes to a SPI device.

Received bytes on the SPI bus are discarded.

Parameters
spiBase address of the SPI instance.
datadata buffer to write
lenLength of data
Precondition
SPI device must be selected with spi_select_device() first

References spi_is_rx_full(), spi_write_single(), and STATUS_OK.

static __always_inline void spi_write_single ( SPI_t *  spi,
uint8_t  data 
)
static

Write one byte to a SPI device.

Parameters
spiBase address of the SPI instance.
dataThe data byte to be loaded

References spi_put().

Referenced by spi_read_packet(), spi_write_packet(), ssd1306_write_command(), and ssd1306_write_data().