This is the unit test application for Monochrome graphical display system. It tests that drawing different primitives will result in the correct output to a display using a framebuffer in RAM.
All AVR devices can be used. This example has been tested with the following setup:
See the documentation for the individual test functions here for detailed descriptions of the tests.
Relevant module dependencies for this application are:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.
Support and FAQ: https://www.microchip.com/support/