Microchip® Advanced Software Framework

unit_tests.c File Reference

Unit tests for graphical drawing primitives.

Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.

#include <stdint.h>
#include <stdbool.h>
#include <stdio.h>
#include <string.h>
#include <asf.h>
#include <conf_test.h>

Functions

int main (void)
 Run gfx_mono unit tests. More...
 
static void run_clear_display_test (const struct test_case *test)
 Test clearing the display. More...
 
static void run_draw_circle_outline_test (const struct test_case *test)
 Test drawing the outline of a circle on a page. More...
 
static void run_draw_diagonal_line_test (const struct test_case *test)
 Test drawing a line between to points. More...
 
static void run_draw_filled_circle_test (const struct test_case *test)
 Test drawing a filled circle spanning two pages. More...
 
static void run_draw_filled_rectangle_test (const struct test_case *test)
 Test drawing a filled rectangle inside a page. More...
 
static void run_draw_flash_bitmap_test (const struct test_case *test)
 Test drawing a bitmap stored in FLASH. More...
 
static void run_draw_horizontal_line_test (const struct test_case *test)
 Test drawing a horizontal line. More...
 
static void run_draw_ram_bitmap_test (const struct test_case *test)
 Test drawing a bitmap stored in RAM. More...
 
static void run_draw_rectangle_outline_test (const struct test_case *test)
 Test drawing the outline of a rectangle spanning two pages. More...
 
static void run_draw_rectangle_two_pages_test (const struct test_case *test)
 Test drawing a filled rectangle spanning two pages. More...
 
static void run_draw_rectangles_test (const struct test_case *test)
 Test drawing a filled rectangle to the every other page of the display. More...
 
static void run_draw_vertical_line_test (const struct test_case *test)
 Test drawing a vertical line. More...
 
static void run_set_display_test (const struct test_case *test)
 Test filling the display. More...
 

Helper functions, macros and bitmaps

#define set_buffer(buffer, value)   memset(buffer, value, sizeof(buffer))
 Set all bytes in buffer to value. More...
 
#define LCD_PAGE_HEIGHT   8
 The height of one lcd page. More...
 
uint8_t smiley_data [16]
 Bitmap of two 8x8 pixel smileyfaces on top of each other stored in RAM. More...
 
 PROGMEM_DECLARE (gfx_mono_color_t, flash_bitmap[16])
 Bitmap of two 8x8 pixel smileyfaces on top of each other stored in FLASH. More...
 
static bool is_page_correct (uint8_t *test_page, uint8_t *correct_page)
 Check if a page buffer is equal to another. More...
 

#define LCD_PAGE_HEIGHT   8

The height of one lcd page.

Referenced by run_draw_rectangles_test().

static bool is_page_correct ( uint8_t *  test_page,
uint8_t *  correct_page 
)
static
PROGMEM_DECLARE ( gfx_mono_color_t  ,
flash_bitmap  [16] 
)

Bitmap of two 8x8 pixel smileyfaces on top of each other stored in FLASH.

static void run_clear_display_test ( const struct test_case test)
static

Test clearing the display.

This test clears the display, and then checks that each page is empty.

Parameters
testCurrent test case.

References gfx_mono_draw_filled_rect, gfx_mono_get_page, GFX_MONO_LCD_HEIGHT, GFX_MONO_LCD_PAGES, GFX_MONO_LCD_WIDTH, GFX_PIXEL_CLR, is_page_correct(), set_buffer, and test_assert_true.

Referenced by main().

static void run_draw_circle_outline_test ( const struct test_case test)
static

Test drawing the outline of a circle on a page.

This test draws the outline of a circle and checks that this is done.

Parameters
testCurrent test case.

References gfx_mono_draw_circle, gfx_mono_draw_filled_rect, gfx_mono_get_page, GFX_MONO_LCD_HEIGHT, GFX_MONO_LCD_PAGES, GFX_MONO_LCD_WIDTH, GFX_PIXEL_CLR, GFX_PIXEL_SET, GFX_WHOLE, is_page_correct(), set_buffer, and test_assert_true.

Referenced by main().

static void run_draw_diagonal_line_test ( const struct test_case test)
static

Test drawing a line between to points.

This test draws a line between two points and checks that this is done.

Parameters
testCurrent test case.

References gfx_mono_draw_filled_rect, gfx_mono_draw_line, gfx_mono_get_page, GFX_MONO_LCD_HEIGHT, GFX_MONO_LCD_PAGES, GFX_MONO_LCD_WIDTH, GFX_PIXEL_CLR, GFX_PIXEL_SET, is_page_correct(), set_buffer, and test_assert_true.

Referenced by main().

static void run_draw_filled_circle_test ( const struct test_case test)
static

Test drawing a filled circle spanning two pages.

This test draws a filled circle spanning two pages and checks that this is done.

Parameters
testCurrent test case.

References gfx_mono_draw_filled_circle, gfx_mono_draw_filled_rect, gfx_mono_get_page, GFX_MONO_LCD_HEIGHT, GFX_MONO_LCD_PAGES, GFX_MONO_LCD_WIDTH, GFX_PIXEL_CLR, GFX_PIXEL_SET, GFX_WHOLE, is_page_correct(), set_buffer, and test_assert_true.

Referenced by main().

static void run_draw_filled_rectangle_test ( const struct test_case test)
static

Test drawing a filled rectangle inside a page.

This test draws a filled rectangle inside a page and checks that this is done.

Parameters
testCurrent test case.

References gfx_mono_draw_filled_rect, gfx_mono_get_page, GFX_MONO_LCD_HEIGHT, GFX_MONO_LCD_PAGES, GFX_MONO_LCD_WIDTH, GFX_PIXEL_CLR, GFX_PIXEL_SET, is_page_correct(), set_buffer, and test_assert_true.

Referenced by main().

static void run_draw_flash_bitmap_test ( const struct test_case test)
static

Test drawing a bitmap stored in FLASH.

This test draws a bitmap to position x = 60, y = 9 and checks that it is aligned with display pages and that it is drawn correctly.

Parameters
testCurrent test case.

References gfx_mono_bitmap::data, GFX_MONO_BITMAP_PROGMEM, gfx_mono_draw_filled_rect, gfx_mono_get_page, GFX_MONO_LCD_HEIGHT, GFX_MONO_LCD_PAGES, GFX_MONO_LCD_WIDTH, gfx_mono_put_bitmap, GFX_PIXEL_CLR, gfx_mono_bitmap::height, is_page_correct(), gfx_mono_bitmap::progmem, set_buffer, test_assert_true, gfx_mono_bitmap::type, and gfx_mono_bitmap::width.

Referenced by main().

static void run_draw_horizontal_line_test ( const struct test_case test)
static

Test drawing a horizontal line.

This test draws a horizontal line and checks that this is done.

Parameters
testCurrent test case.

References gfx_mono_draw_filled_rect, gfx_mono_draw_horizontal_line, gfx_mono_get_page, GFX_MONO_LCD_HEIGHT, GFX_MONO_LCD_PAGES, GFX_MONO_LCD_WIDTH, GFX_PIXEL_CLR, GFX_PIXEL_SET, is_page_correct(), set_buffer, and test_assert_true.

Referenced by main().

static void run_draw_ram_bitmap_test ( const struct test_case test)
static

Test drawing a bitmap stored in RAM.

This test draws a bitmap to position x = 50, y = 5 and checks that it is aligned with display pages and that it is drawn correctly.

Parameters
testCurrent test case.

References gfx_mono_bitmap::data, GFX_MONO_BITMAP_RAM, gfx_mono_draw_filled_rect, gfx_mono_get_page, GFX_MONO_LCD_HEIGHT, GFX_MONO_LCD_PAGES, GFX_MONO_LCD_WIDTH, gfx_mono_put_bitmap, GFX_PIXEL_CLR, gfx_mono_bitmap::height, is_page_correct(), gfx_mono_bitmap::pixmap, set_buffer, smiley_data, test_assert_true, gfx_mono_bitmap::type, and gfx_mono_bitmap::width.

Referenced by main().

static void run_draw_rectangle_outline_test ( const struct test_case test)
static

Test drawing the outline of a rectangle spanning two pages.

This test draws the outline of a rectangle spanning two pages and checks that this is done.

Parameters
testCurrent test case.

References gfx_mono_draw_filled_rect, gfx_mono_draw_rect, gfx_mono_get_page, GFX_MONO_LCD_HEIGHT, GFX_MONO_LCD_PAGES, GFX_MONO_LCD_WIDTH, GFX_PIXEL_CLR, GFX_PIXEL_SET, is_page_correct(), set_buffer, and test_assert_true.

Referenced by main().

static void run_draw_rectangle_two_pages_test ( const struct test_case test)
static

Test drawing a filled rectangle spanning two pages.

This test draws a filled rectangle spanning two pages and checks that this is done.

Parameters
testCurrent test case.

References gfx_mono_draw_filled_rect, gfx_mono_get_page, GFX_MONO_LCD_HEIGHT, GFX_MONO_LCD_PAGES, GFX_MONO_LCD_WIDTH, GFX_PIXEL_CLR, GFX_PIXEL_SET, is_page_correct(), set_buffer, and test_assert_true.

Referenced by main().

static void run_draw_rectangles_test ( const struct test_case test)
static

Test drawing a filled rectangle to the every other page of the display.

This test draws a filled rectangle to every other page of a display and checks that every other page is filled and the rest are empty.

Parameters
testCurrent test case.

References gfx_mono_draw_filled_rect, gfx_mono_get_page, GFX_MONO_LCD_HEIGHT, GFX_MONO_LCD_PAGES, GFX_MONO_LCD_WIDTH, GFX_PIXEL_CLR, GFX_PIXEL_SET, is_page_correct(), LCD_PAGE_HEIGHT, set_buffer, and test_assert_true.

Referenced by main().

static void run_draw_vertical_line_test ( const struct test_case test)
static

Test drawing a vertical line.

This test draws a vertical line and checks that this is done.

Parameters
testCurrent test case.

References gfx_mono_draw_filled_rect, gfx_mono_draw_vertical_line, gfx_mono_get_page, GFX_MONO_LCD_HEIGHT, GFX_MONO_LCD_PAGES, GFX_MONO_LCD_WIDTH, GFX_PIXEL_CLR, GFX_PIXEL_SET, is_page_correct(), set_buffer, and test_assert_true.

Referenced by main().

static void run_set_display_test ( const struct test_case test)
static

Test filling the display.

This test fills the entire display and checks that this is done.

Parameters
testCurrent test case.

References gfx_mono_draw_filled_rect, gfx_mono_get_page, GFX_MONO_LCD_HEIGHT, GFX_MONO_LCD_PAGES, GFX_MONO_LCD_WIDTH, GFX_PIXEL_CLR, GFX_PIXEL_SET, is_page_correct(), set_buffer, and test_assert_true.

Referenced by main().

uint8_t smiley_data[16]
Initial value:
= {
0x3C, 0x42, 0x95, 0xA1, 0xA1, 0x95, 0x42, 0x3C,
0x3C, 0x42, 0x95, 0xA1, 0xA1, 0x95, 0x42, 0x3C
}

Bitmap of two 8x8 pixel smileyfaces on top of each other stored in RAM.

Referenced by run_draw_ram_bitmap_test().