This is the unit test application for the Spinner widget for monochrome graphical displays. It tests that the a set of keycodes processed by a spincollection results in expected spinner choices.
All AVR devices can be used. This example has been tested with the following setup:
See the documentation for the individual test functions here for detailed descriptions of the tests.
Relevant module dependencies for this application are:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.