AKM AK8975 3-axis magnetometer.
This file contains functions for initializing and reading data from a AKM AK8975 3-axis magnetometer.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | SELF_TEST_DELAY (0x80000) |
Delay loop count during self-test. More... | |
Functions | |
static void | ak8975_apply_offset (vector3_t *input) |
Apply stored offset values to sensor reading. More... | |
static bool | ak8975_calibrate (sensor_t *sensor, sensor_calibration_t calib_type, int step, void *info) |
Calibrate magnetometer. More... | |
static bool | ak8975_check_overflow (const vector3_t *data) |
@ brief Test for magnetic sensor overflow More... | |
static bool | ak8975_device_id (sensor_hal_t *hal, sensor_data_t *data) |
Read magnetometer device ID. More... | |
static bool | ak8975_get_data (sensor_hal_t *hal, uint8_t mode, vector3_t *data) |
Read magnetometer vector data. More... | |
static bool | ak8975_get_field (sensor_hal_t *hal, sensor_data_t *data) |
Read magnetometer vector (3-axis) data. More... | |
static bool | ak8975_get_heading (sensor_hal_t *hal, sensor_data_t *data) |
Read magnetometer heading/direction data. More... | |
bool | ak8975_init (sensor_t *sensor, int resvd) |
AKM AK8975 magnetometer driver initialization. More... | |
static bool | ak8975_ioctl (sensor_t *sensor, sensor_command_t cmd, void *arg) |
AK8975 ioctl control entry point. More... | |
static bool | ak8975_read (sensor_t *sensor, sensor_read_t type, sensor_data_t *data) |
Read sensor data. More... | |
static bool | ak8975_selftest (sensor_t *sensor, int *test_code, void *arg) |
Perform self-test function. More... | |
static bool | ak8975_set_state (sensor_hal_t *hal, sensor_state_t state) |
AKM AK8975 device state set routine. More... | |
Variables | |
static vector3_t | calibrated_offsets |
Sensor Calibration Data. More... | |
#define SELF_TEST_DELAY (0x80000) |
Delay loop count during self-test.
Referenced by ak8975_selftest().
|
inlinestatic |
Apply stored offset values to sensor reading.
This function applies stored calibration offsets to the "input" vector of magnetometer values (the magnetic field vector) and returns the modified values.
input | Contains the measured magnetic field values. The offset-adjusted values will replace the contents. |
true | successfully adjusted sensor readings |
false | Failed to adjust sensor readings |
References vector3_t::x, vector3_t::y, and vector3_t::z.
Referenced by ak8975_get_field(), and ak8975_get_heading().
|
static |
Calibrate magnetometer.
This function measures the magnetometer output if 3 different device orientations, calculates average offset values, and stores these offsets in non-volatile memory. The offsets will later be used during normal measurements, to compensate for fixed magnetic effects.
This routine must be called 3 times total, with the "step" parameter indicating what stage of the calibration is being performed. This multi-step mechanism allows the application to prompt for physical placement of the sensor device before this routine is called.
sensor | Address of an initialized sensor device descriptor. |
calib_type | The address of a vector storing sensor axis data. |
step | The calibration stage number [1,3]. |
info | Unimplemented (ignored) parameter. |
References ak8975_check_overflow(), ak8975_get_data(), AK8975_SINGLE_MODE, sensor_desc::err, sensor_desc::hal, MANUAL_CALIBRATE, nvram_read(), nvram_write(), SENSOR_ERR_IO, SENSOR_ERR_PARAMS, vector3_t::x, vector3_t::y, and vector3_t::z.
Referenced by ak8975_init().
@ brief Test for magnetic sensor overflow
AK8975/B has the limitation for measurement range that the sum of the absolute values of each axis should be smaller than 2400 microtesla:
|x| + |y| + |z| < 2400 uT
When the magnetic field exceeds this limitation, data stored at measurement data are not correct. This is called "Magnetic Sensor Overflow".
When magnetic sensor overflow occurs, HOFL but turns to "1". When the next measurement starts, it returns to "0".
References AK8975_DATA_RESOLUTION, MICRO_TESLA_PER_COUNT, vector3_t::x, vector3_t::y, and vector3_t::z.
Referenced by ak8975_calibrate(), ak8975_get_field(), and ak8975_get_heading().
|
static |
Read magnetometer device ID.
This function reads the magnetometer hardware identification registers and returns these values to the addresses specified in the function parameters.
hal | Address of an initialized sensor hardware descriptor. |
data | Address of sensor_data_t structure to return values. |
References AK8975_REG_WIA, sensor_data_t::device, and sensor_bus_get.
Referenced by ak8975_read().
|
static |
Read magnetometer vector data.
This function obtains magnetometer data for all three axes of the AKM device. The data is read from six device registers using a multi-byte bus transfer. The 13-bit raw results are then assembled from the two register values for each axis, including extending the sign bit, to form a signed 16-bit value.
hal | Address of an initialized sensor hardware descriptor. |
data | The address of a vector storing sensor axis data. |
References AK8975_REG_CNTL1, AK8975_REG_HXL, sensor_axis_vec_t::axis, gpio_pin_is_low, sensor_hal::mcu_sigint, sensor_hal::orientation, sensor_bus_put, sensor_bus_read, sensor_axis_vec_t::sign, vector3_t::x, sensor_orient_t::x, vector3_t::y, sensor_orient_t::y, vector3_t::z, and sensor_orient_t::z.
Referenced by ak8975_calibrate(), ak8975_get_field(), ak8975_get_heading(), and ak8975_selftest().
|
static |
Read magnetometer vector (3-axis) data.
This function obtains magnetometer data for all three axes of the AKM device. The data is read from six device registers using a multi-byte bus transfer. The 10-bit raw results are then assembled from the two register values for each axis, including extending the sign bit, to form a signed 32-bit value.
Along with the actual sensor data, the LSB byte contains a "new" flag indicating if the data for this axis has been updated since the last time the axis data was read. Reading either LSB or MSB data will clear this flag.
hal | Address of an initialized sensor hardware descriptor. |
data | The address of a vector storing sensor axis data. |
References ak8975_apply_offset(), ak8975_check_overflow(), ak8975_get_data(), AK8975_SINGLE_MODE, sensor_data_t::axis, MICRO_TESLA_PER_COUNT, sensor_data_t::scaled, vector3_scale(), vector3_t::x, vector3_t::y, and vector3_t::z.
Referenced by ak8975_read().
|
static |
Read magnetometer heading/direction data.
This function obtains magnetometer data for all three axes of the AKM device. The data is read from six device registers using a multi-byte bus transfer. The 10-bit raw results are then assembled from the two register values for each axis, including extending the sign bit, to form a signed 32-bit value.
Along with the actual sensor data, the LSB byte contains a "new" flag indicating if the data for this axis has been updated since the last time the axis data was read. Reading either LSB or MSB data will clear this flag.
hal | Address of an initialized sensor hardware descriptor. |
data | The address of a vector storing sensor axis data. |
References ak8975_apply_offset(), ak8975_check_overflow(), ak8975_get_data(), AK8975_SINGLE_MODE, field_direction(), sensor_data_t::heading, and MICRO_TESLA_PER_COUNT.
Referenced by ak8975_read().
AKM AK8975 magnetometer driver initialization.
This is the main initialization function for the AK8975 device.
sensor | Address of a sensor device descriptor. |
resvd | Reserved value. |
References ak8975_calibrate(), AK8975_DATA_RESOLUTION, ak8975_ioctl(), ak8975_read(), AK8975_REG_WIA, ak8975_selftest(), AK8975_WIA_VALUE, sensor_desc::drv, sensor_device_t::func, sensor_desc::hal, nvram_read(), sensor_funcs_t::read, sensor_hal::resolution, sensor_bus_get, SENSOR_CAPS_3_AXIS, SENSOR_CAPS_SELFTEST, SENSOR_SCALE_micro, SENSOR_UNITS_tesla, SENSOR_VENDOR_AKM, vector3_t::x, vector3_t::y, and vector3_t::z.
|
static |
AK8975 ioctl control entry point.
hal | Address of an initialized sensor hardware descriptor. |
cmd | Command to execute |
arg | Argument for command (varies) |
References ak8975_set_state(), sensor_desc::err, sensor_desc::hal, SENSOR_ERR_UNSUPPORTED, SENSOR_SET_STATE, and status.
Referenced by ak8975_init().
|
static |
Read sensor data.
This routine calls the appropriate internal data function to obtain the specified type of data from the sensor device.
sensor | Address of an initialized sensor device descriptor. |
type | Type of sensor data to read. |
data | The address where data values are returned. |
References ak8975_device_id(), ak8975_get_field(), ak8975_get_heading(), sensor_desc::err, sensor_desc::hal, SENSOR_ERR_FUNCTION, SENSOR_READ_FIELD, SENSOR_READ_HEADING, and SENSOR_READ_ID.
Referenced by ak8975_init().
Perform self-test function.
This function sets up and executes the built-in self test function of the AK8975 sensor device.
test_code | Address of a numeric code of which test to perform This location will contain the specific test result code when the function returns. |
References AK8975_ASTC_SELF, ak8975_get_data(), AK8975_POWER_DOWN_MODE, AK8975_REG_ASTC, AK8975_REG_CNTL1, AK8975_SELF_TEST_MODE, AK8975_TEST_X_MAX, AK8975_TEST_X_MIN, AK8975_TEST_Y_MAX, AK8975_TEST_Y_MIN, AK8975_TEST_Z_MAX, AK8975_TEST_Z_MIN, sensor_desc::hal, SELF_TEST_DELAY, sensor_bus_put, SENSOR_TEST_ERR_NONE, SENSOR_TEST_ERR_RANGE, SENSOR_TEST_ERR_READ, vector3_t::x, vector3_t::y, and vector3_t::z.
Referenced by ak8975_init().
|
static |
AKM AK8975 device state set routine.
This function places the AK8975 device in the specified state.
sensor | Address of a sensor device descriptor. |
state | State device will be placed into. |
References AK8975_POWER_DOWN_MODE, AK8975_REG_CNTL1, sensor_bus_put, SENSOR_STATE_POWER_DOWN, and SENSOR_STATE_SLEEP.
Referenced by ak8975_ioctl().
|
static |
Sensor Calibration Data.
This variable stores copies of axis calibration offsets stored in NVRAM.
The current implementation will either use software floating-point routines from the toolchain or fixed-point math routines in the ASF. All fractional sensor data should use types defined in precision.h where the type scalar_t
is an alias for a C/C++ floating-point type or an integer type used by fixed-point arithmetic functions defined in the API.