Sensor platform unit test.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
static void | configure_sensor_platform (void) |
Initializes the sensor platform - as this calls the board and sysclock init functions internally, it will also wait for any pending serial transfer(s) to complete before calling sensor_platform_init() and will re-initialize the USART afterwards to ensure no corrupt or lost data. More... | |
int | main (void) |
static void | run_sensor_accel_test (const struct test_case *test) |
Unit test to check that the accelerometer works correctly on the Inertial One board using the Sensor Platform library. More... | |
static void | run_sensor_compass_test (const struct test_case *test) |
Unit test to check that the compass works correctly on the Inertial One board using the Sensor Platform library. More... | |
static void | run_sensor_gyro_test (const struct test_case *test) |
Unit test to check that the gyroscope works correctly on the Inertial One board using the Sensor Platform library. More... | |
static void | run_sensor_init_test (const struct test_case *test) |
Unit test to check that the Sensor Platform is initialized correctly with the Intertial One board. More... | |
static void | run_sensor_temp_test (const struct test_case *test) |
Unit test to check that the gyroscope internal temperature sensor works correctly on the Inertial One board using the Sensor Platform library. More... | |
Variables | |
static const usart_serial_options_t | usart_serial_options |
|
static |
Initializes the sensor platform - as this calls the board and sysclock init functions internally, it will also wait for any pending serial transfer(s) to complete before calling sensor_platform_init() and will re-initialize the USART afterwards to ensure no corrupt or lost data.
References CONF_TEST_USART, sensor_platform_init(), stdio_serial_init(), and usart_tx_empty().
Referenced by run_sensor_accel_test(), run_sensor_compass_test(), run_sensor_gyro_test(), run_sensor_init_test(), and run_sensor_temp_test().
int main | ( | void | ) |
|
static |
Unit test to check that the accelerometer works correctly on the Inertial One board using the Sensor Platform library.
test | Pointer to the unit test case instance |
References sensor_data_t::axis, configure_sensor_platform(), delay_ms, sensor_desc::err, sensor_data_t::scaled, sensor_attach(), sensor_get_acceleration(), SENSOR_TYPE_ACCELEROMETER, test_assert_false, test_assert_true, vector3_magnitude(), vector3_t::x, vector3_t::y, and vector3_t::z.
Referenced by main().
|
static |
Unit test to check that the compass works correctly on the Inertial One board using the Sensor Platform library.
test | Pointer to the unit test case instance |
References configure_sensor_platform(), delay_ms, sensor_desc::err, sensor_data_t::heading, sensor_data_t::scaled, sensor_attach(), sensor_get_heading(), SENSOR_TYPE_COMPASS, test_assert_false, test_assert_true, vector3_magnitude(), vector3_t::x, vector3_t::y, and vector3_t::z.
Referenced by main().
|
static |
Unit test to check that the gyroscope works correctly on the Inertial One board using the Sensor Platform library.
test | Pointer to the unit test case instance |
References configure_sensor_platform(), delay_ms, sensor_desc::err, sensor_data_t::scaled, sensor_attach(), sensor_get_rotation(), SENSOR_TYPE_GYROSCOPE, test_assert_false, and test_assert_true.
Referenced by main().
|
static |
Unit test to check that the Sensor Platform is initialized correctly with the Intertial One board.
test | Pointer to the unit test case instance |
References configure_sensor_platform(), sensor_desc::err, sensor_attach(), SENSOR_TYPE_ACCELEROMETER, SENSOR_TYPE_COMPASS, SENSOR_TYPE_GYROSCOPE, and test_assert_false.
Referenced by main().
|
static |
Unit test to check that the gyroscope internal temperature sensor works correctly on the Inertial One board using the Sensor Platform library.
test | Pointer to the unit test case instance |
References configure_sensor_platform(), delay_ms, sensor_desc::err, sensor_data_t::scaled, sensor_attach(), sensor_get_temperature(), SENSOR_TYPE_GYROSCOPE, sensor_data_t::temperature, test_assert_false, and test_assert_true.
Referenced by main().
|
static |