Microchip® Advanced Software Framework

ui.h File Reference

Common User Interface for USB host Android Open Accessory Protocol.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

#include "uhc.h"

Macros

Commands from accessory to Android device
#define MESSAGE_ATD_SIMPLE_SWITCH   0x01
 
#define MESSAGE_ATD_SENSOR_TEMPERATURE   0x10
 
#define MESSAGE_ATD_SENSOR_LIGHT   0x11
 
Commands from Android device to accessory
#define MESSAGE_DTA_SIMPLE_LED   0x02
 
#define MESSAGE_DTA_SIMPLE_DISPLAY_BACKLIGHT   0x03
 
#define MESSAGE_DTA_STRING_BASIC   0x20
 

Functions

void read_complete (usb_add_t add, usb_ep_t ep, uhd_trans_status_t, iram_size_t)
 Called when Bulk IN Transfer is finished. More...
 
void ui_init (void)
 Initializes the user interface. More...
 
void ui_uhi_aoa_change (uhc_device_t *dev, bool b_plug)
 
void ui_usb_connection_event (uhc_device_t *dev, bool b_present)
 Notify that a USB device has been connected or disconnected. More...
 
void ui_usb_enum_event (uhc_device_t *dev, uhc_enum_status_t status)
 Notify the end of a USB device enumeration process. More...
 
void ui_usb_message_reception (void)
 Processing of a Message from the Android device. More...
 
void ui_usb_mode_change (bool b_host_mode)
 Notify that the USB mode is switched automatically. This is only possible when the ID pin is available. More...
 
void ui_usb_sof_event (void)
 Notify that a SOF has been sent (each 1 ms) More...
 
void ui_usb_vbus_change (bool b_vbus_present)
 Notify that a Vbus is changed Available only in USB hardware with Vbus monitoring. More...
 
void ui_usb_vbus_error (void)
 Notify that a Vbus error has occurred Available only in USB hardware with Vbus monitoring. More...
 
void ui_usb_wakeup_event (void)
 Notify that a USB device or the host woke up the USB line. More...
 

#define MESSAGE_ATD_SENSOR_LIGHT   0x11

Referenced by ui_adc_read().

#define MESSAGE_ATD_SENSOR_TEMPERATURE   0x10
#define MESSAGE_ATD_SIMPLE_SWITCH   0x01

Referenced by ui_usb_sof_event().

#define MESSAGE_DTA_SIMPLE_DISPLAY_BACKLIGHT   0x03
#define MESSAGE_DTA_SIMPLE_LED   0x02
#define MESSAGE_DTA_STRING_BASIC   0x20

void ui_init ( void  )
void ui_uhi_aoa_change ( uhc_device_t *  dev,
bool  b_plug 
)

References ui_aoa_plug.

void ui_usb_connection_event ( uhc_device_t *  dev,
bool  b_present 
)

Notify that a USB device has been connected or disconnected.

Parameters
devPointer on USB device information
b_presenttrue, if the device has been connected

References uhi_aoa_uninstall(), ui_display_init_rtc(), ui_display_welcome_msg(), and ui_enum_status.

void ui_usb_enum_event ( uhc_device_t *  dev,
uhc_enum_status_t  status 
)

Notify the end of a USB device enumeration process.

Parameters
devPointer on USB device information
statusStatus of the USB enumeration

References BLACK, BLUE, et024006_DrawFilledRect(), ET024006_HEIGHT, et024006_PrintString(), ET024006_WIDTH, FONT8x16, ui_button_rtc_init(), ui_display_disable_rtc(), ui_display_draw_textbox(), ui_enum_status, and WHITE.

void ui_usb_mode_change ( bool  b_host_mode)

Notify that the USB mode is switched automatically. This is only possible when the ID pin is available.

Parameters
b_host_modetrue, if the host mode has been selected

References LED3, LED_Off(), and LED_On().

void ui_usb_vbus_change ( bool  b_vbus_present)

Notify that a Vbus is changed Available only in USB hardware with Vbus monitoring.

Parameters
b_vbus_presenttrue, if Vbus is high.
void ui_usb_vbus_error ( void  )

Notify that a Vbus error has occurred Available only in USB hardware with Vbus monitoring.

void ui_usb_wakeup_event ( void  )

Notify that a USB device or the host woke up the USB line.