License | Subject to your compliance with these terms, you may use Microchip software and any derivatives exclusively with Microchip products |
Quick start guide for the SAM USART module | This is the quick start guide for the USART module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
USART receive character and echo back | In this use case, the USART module is configured for: |
USART receive character and echo back via interrupts | In this use case, the USART module is configured for: |
Quick Start Guide for the System Clock Management service (SAM4S) | This is the quick start guide for the System Clock Management service, with step-by-step instructions on how to configure and use the service for specific use cases |
Advanced use case - Peripheral Bus Clock Management (SAM4S) | |
Quick start guide for the SAM PMC module | This is the quick start guide for the PMC module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick start guide for USB device Communication Class Device module (UDI CDC) | This is the quick start guide for the USB device interface CDC module (UDI CDC) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
CDC in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
Change USB speed | In this use case, the USB device is used with different USB speeds |
Use USB strings | In this use case, the usual USB strings is added in the USB device |
Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
USB dynamic serial number | In this use case, the USB serial strings is dynamic |
conf_clock.h examples with USB support | Content of XMEGA conf_clock.h: |
Quick start guide for the common IOPORT service | This is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases |
Advanced use case doing port access | In this case we will read out the pins from one whole port and write the read value to another port |
Quick Start Guide for the SAM PIO driver | This is the quick start guide for the PIO Driver, with step-by-step instructions on how to configure and use the driver for specific use cases |
Advanced use case - Interrupt driven edge detection | |
"SAM4S-EK - Operating frequencies" | This page lists several definition related to the board operating frequency |
"SAM4S-EK - Board informations" | This page lists several definition related to the board description |
"SAM4S-EK - USB device" | |
"SAM4S-EK - External components" | This page lists the definitions related to external on-board components located in the board.h file for the SAM4S-EK |
"SAM4S-EK - Memories" | This page lists definitions related to internal & external on-board memories |
Todo List | |