User Interface.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | ui_com_close (uint8_t port) |
Called when communication port is closed. More... | |
void | ui_com_error (void) |
Called when a communication error occur. More... | |
void | ui_com_open (uint8_t port) |
Called when communication port is opened. More... | |
void | ui_com_overflow (void) |
Called when a overflow occur. More... | |
void | ui_com_rx_start (void) |
Called when a data is received on CDC. More... | |
void | ui_com_rx_stop (void) |
Called when all data pending are sent on port com. More... | |
void | ui_com_tx_start (void) |
Called when a data is received on port com. More... | |
void | ui_com_tx_stop (void) |
Called when all data pending are sent on CDC. More... | |
void | ui_init (void) |
Called at firmware startup. More... | |
void | ui_powerdown (void) |
Called before enter in powerdown mode. More... | |
void | ui_process (uint16_t framenumber) |
This process is called each 1ms It is called only if the USB interface is enabled. More... | |
void | ui_wakeup (void) |
Called when CPU exit of powerdown mode. More... | |
void ui_com_close | ( | uint8_t | port | ) |
Called when communication port is closed.
References LED1_GPIO, and LED_Off().
Referenced by main_cdc_set_dtr().
void ui_com_error | ( | void | ) |
Called when a communication error occur.
Referenced by usart_handler().
void ui_com_open | ( | uint8_t | port | ) |
Called when communication port is opened.
References LED1_GPIO, and LED_On().
Referenced by main_cdc_set_dtr().
void ui_com_overflow | ( | void | ) |
Called when a overflow occur.
Referenced by usart_handler().
void ui_com_rx_start | ( | void | ) |
Called when a data is received on CDC.
Referenced by usart_handler().
void ui_com_rx_stop | ( | void | ) |
Called when all data pending are sent on port com.
Referenced by usart_handler().
void ui_com_tx_start | ( | void | ) |
Called when a data is received on port com.
Referenced by usart_handler().
void ui_com_tx_stop | ( | void | ) |
Called when all data pending are sent on CDC.
Referenced by usart_handler().
void ui_init | ( | void | ) |
void ui_powerdown | ( | void | ) |
Called before enter in powerdown mode.
References LED0_GPIO, LED1_GPIO, and LED_Off().
Referenced by main(), and main_suspend_action().
void ui_process | ( | uint16_t | framenumber | ) |
This process is called each 1ms It is called only if the USB interface is enabled.
framenumber | Current frame number |
References LED0_GPIO, LED_Off(), and LED_On().
Referenced by main_sof_action().
void ui_wakeup | ( | void | ) |
Called when CPU exit of powerdown mode.
References LED0_GPIO, and LED_On().
Referenced by main_resume_action().