User Interface.
Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | MOUSE_MOVE_RANGE 3 |
Functions | |
ISR (ui_wakeup_isr, AVR32_GPIO_IRQ_GROUP, 0) | |
void | ui_init (void) |
Initializes the user interface. More... | |
void | ui_powerdown (void) |
Sets the user interface in power down mode. More... | |
void | ui_process (uint16_t framenumber) |
This process is called each 1ms It is called only if the USB interface is enabled. More... | |
void | ui_start_read (void) |
void | ui_start_write (void) |
void | ui_stop_read (void) |
void | ui_stop_write (void) |
void | ui_wakeup (void) |
Exits the user interface of power down mode. More... | |
void | ui_wakeup_disable (void) |
Disables the asynchronous interrupts of the user interface. More... | |
void | ui_wakeup_enable (void) |
Enables the asynchronous interrupts of the user interface. More... | |
Variables | |
static const eic_options_t | eic_options |
Structure holding the configuration parameters of the EIC low level driver. More... | |
#define MOUSE_MOVE_RANGE 3 |
Referenced by ui_process().
ISR | ( | ui_wakeup_isr | , |
AVR32_GPIO_IRQ_GROUP | , | ||
0 | |||
) |
void ui_init | ( | void | ) |
Initializes the user interface.
References cpu_irq_restore(), cpu_irq_save(), GPIO_JOYSTICK_PUSH, irq_register_handler, LED0, LED1, LED_Off(), and LED_On().
Referenced by main().
void ui_powerdown | ( | void | ) |
Sets the user interface in power down mode.
References LED0, LED1, and LED_Off().
Referenced by main(), and main_suspend_action().
void ui_process | ( | uint16_t | framenumber | ) |
This process is called each 1ms It is called only if the USB interface is enabled.
framenumber | Current frame number |
References gpio_get_pin_value(), GPIO_PUSH_BUTTON_0, GPIO_PUSH_BUTTON_1, GPIO_PUSH_BUTTON_2, HID_MOUSE_BTN_DOWN, HID_MOUSE_BTN_UP, is_joystick_down(), is_joystick_left(), is_joystick_right(), is_joystick_up(), LED1, LED_Off(), LED_On(), MOUSE_MOVE_RANGE, udi_hid_mouse_btnleft(), udi_hid_mouse_btnmiddle(), udi_hid_mouse_btnright(), udi_hid_mouse_moveX(), and udi_hid_mouse_moveY().
Referenced by main_sof_action().
void ui_start_read | ( | void | ) |
References LED_BI0_GREEN, and LED_On().
void ui_start_write | ( | void | ) |
References LED_BI0_RED, and LED_On().
void ui_stop_read | ( | void | ) |
References LED_BI0_GREEN, and LED_Off().
void ui_stop_write | ( | void | ) |
References LED_BI0_RED, and LED_Off().
void ui_wakeup | ( | void | ) |
Exits the user interface of power down mode.
References LED0, and LED_On().
Referenced by main_resume_action().
void ui_wakeup_disable | ( | void | ) |
Disables the asynchronous interrupts of the user interface.
References eic_disable_line(), EXT_NMI, gpio_disable_pin_interrupt(), and GPIO_JOYSTICK_PUSH.
Referenced by main_remotewakeup_disable().
void ui_wakeup_enable | ( | void | ) |
Enables the asynchronous interrupts of the user interface.
References eic_enable_line(), eic_init(), EXT_NMI, gpio_enable_module_pin(), gpio_enable_pin_interrupt(), gpio_enable_pin_pull_up(), GPIO_JOYSTICK_PUSH, and GPIO_PIN_CHANGE.
Referenced by main_remotewakeup_enable().
|
static |
Structure holding the configuration parameters of the EIC low level driver.